cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F753 LWIP stack not initializing after reboot

JohnnyB
Associate II

We're running into what seems to be a low-level race-condition when initializing LWIP on boot. The LWIP always initializes successfully after using the STLink to flash the .elf either in debug and release modes. After flashing, I verify by sending a ping command to the Ethernet interface and get a good response with TTL. I then subsequently cycle the power and ping returns the infamous "Request timed out" message.

It's difficult to debug because the initialization issue goes away once I start a debug session. So, I'm completely in the dark on this one. Any and all help/suggestion/insight is much appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

I solved this problem by adding a HAL_Delay() in main.c before LWIP is initialized. The reason for the delay was based on my hunch of power instability. So, the delay allowed the entire device to reach a steady-state. 

View solution in original post

6 REPLIES 6
Andrew Neil
Super User

@JohnnyB wrote:

It's difficult to debug because the initialization issue goes away once I start a debug session. So, I'm completely in the dark on this one. .


Shine light with, eg, UART output; LEDs to show progress; etc ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thanks. The UART works as we have serial communication with the board and we have onboard LEDs to indicate the board is in a running state. It's just the Ethernet stack is not initialized.

So sprinkle UART status output through the LwIP process - so that you can see progress when the debugger's not connected.

Compare & contrast with when it doesn't work ...

Do the LEDs indicate that the board is in a "running state" when this happens?

 

EDIT:

Not surprisingly, it seems LwIP has printf dbugging built in:

https://lwip.fandom.com/wiki/Debugging_lwIP#:~:text=lwIP%20is%20developed%20with%20some%20nice%20support%20for%20enabling%20various%20debug%20print%20options

 

See also:

https://community.st.com/t5/stm32-mcus-embedded-software/how-to-activate-debug-messages-for-lwip/td-p/234162

 

And:

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Enabling-debug-output/ta-p/1128854 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I solved this problem by adding a HAL_Delay() in main.c before LWIP is initialized. The reason for the delay was based on my hunch of power instability. So, the delay allowed the entire device to reach a steady-state. 

If you're happy with that, then please mark it as the solution.

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Andrew, just wanted to send a quick thank you for promptly chiming in to try to help. Cheers.