2025-03-11 6:18 AM
Hi!
with cube IDE i'm trying to develop a USB device with 3 classes using a STM32H523 with USBX and threadX.
If i select USB HID,USB MSC and USB ACM (virtual com port) the code is succesfully generated but if i close and reopen the .ioc GUI i have this message error:
the value of UX_MAX_DEVICE_ENDPOINTS can't be less then number of endpoints used.(used endpoints: 7). it will be set to 6.
what does it mean? is not possible to have 3 classes? or i have to change something in the endpoints and it can be done?
there is an example like this? or a guide to understande the endspoint manage
thank you
Solved! Go to Solution.
2025-03-12 4:56 AM
Hi @ABasi.2
in stm32h5 the max endpoint is 8
In your project you are using
if you define this endpoints config the problem will dispparate in Mx
ensure that UX_DEVICE_BIDIRECTIONAL_ENDPOINT_SUPPORT is enbled
2025-03-11 7:05 AM
Hi @ABasi.2
Would you attach ioc file to reproduce? Make sure to use latest version.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-11 8:04 AM
2025-03-12 4:56 AM
Hi @ABasi.2
in stm32h5 the max endpoint is 8
In your project you are using
if you define this endpoints config the problem will dispparate in Mx
ensure that UX_DEVICE_BIDIRECTIONAL_ENDPOINT_SUPPORT is enbled
2025-03-13 12:14 AM
Hello Mohamed
thank you!
threre is a manual / video guide ecc about this topic that you know? i 'm new in USB and a want to learn
Is it possible to use the same end point for 2 different classes?
i saw a video from ST : https://www.youtube.com/watch?v=wCRIpp-OHY4&t=167s
where it seems possible if you respect the in and out configuration of endpint
thank you