cancel
Showing results for 
Search instead for 
Did you mean: 

USB read failing in standard 32H743 USB MSC with 16GB pen drive

Robmar
Senior III

A BOT protocol read fail error is occurring in usbh_msc.bot.c:- See "*** MY MOD-" below

USBH_StatusTypeDef USBH_MSC_BOT_Process (USBH_HandleTypeDef *phost, uint8_t lun)
{
...

else if (URB_Status == USBH_URB_STALL)

{

/* This is Data IN Stage STALL Condition */

MSC_Handle->hbot.state = BOT_ERROR_IN;



/* Refer to USB Mass-Storage Class : BOT (www.usb.org)

6.7.2 Host expects to receive data from the device

3. On a STALL condition receiving data, then:

The host shall accept the data received.

The host shall clear the Bulk-In pipe.

4. The host shall attempt to receive a CSW.*/



#if (USBH_USE_OS == 1)

osMessagePut ( phost->os_event, USBH_URB_EVENT, 0);

#endif

}

else if (URB_Status == USBH_URB_ERROR) // *** MY MOD- *** added as getting error here!

{

/* This is Data IN Stage ERROR Condition */

MSC_Handle->hbot.state = BOT_ERROR_IN; // tried this but no change

}

break;



case BOT_DATA_OUT:
...

 

2 REPLIES 2
FBL
ST Employee

Hi @Robmar 

Would you share an example to reproduce the read failure? After all, thank you for highlighting this error handling.  An internal ticket 200414 is submitted to the dedicated team. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
FBL
ST Employee

Hi @Robmar 

Reviewing the code the actual implementation is correct as the part you are highlighting is managed in BOT_ERROR_IN case

    case BOT_ERROR_IN:
      error = USBH_MSC_BOT_Abort(phost, lun, BOT_DIR_IN);

      if (error == USBH_OK)
      {
        MSC_Handle->hbot.state = BOT_RECEIVE_CSW;
      }
      else if (error == USBH_UNRECOVERED_ERROR)
      {
        /* This means that there is a STALL Error limit, Do Reset Recovery */
        MSC_Handle->hbot.state = BOT_UNRECOVERED_ERROR;

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL