2016-09-24 3:00 AM
Does anyone USB Device HID Keyboard example? I'm struggling to modify USB mouse example into keyboard. Read some literature, tried to modify descriptors, but no luck...
#hid #hid #hid #usb-device #device #keyboard #keyboard #usb-hid #consumer2016-09-29 4:52 AM
Hi Tsuneo,
Thank you for your valuable input !Kraal2016-09-29 5:22 AM
Hi Alex,
> Now I'm struggling to make multimedia keys work. 'Multimedia' keys belong to HID consumer device, apart from other keys (HID keyboard). - To send these keys, you have to modify your report descriptor completely for HID consumer device. - If you would like to have 'multimedia' keys with ordinary keys, you should make a composite device, HID keyboard + HID consumer, because Windows don't like merged keyboard with other HID device(s) using TLCs (Top-Level Collections). In this reason, all of PC keyboards are composite devices. The support of 'multimedia' keys depend on OS. Windows support is described on keyboard-support-windows-8.docx, downloaded from this MS page,https://msdn.microsoft.com/en-us/library/windows/hardware/Dn613956%28v=vs.85%aspx
//
// Report descriptor for media remote controller
//
// This descriptor defines ONE byte report, of this bitmap
// bit
// 0 : Next
// 1 : Previous
// 2 : Stop
// 3 : Play/Pause
// 4 : Mute
// 5 : Volume Up
// 6 : Volume Down
// 7 : --- (padding)
//
static u8 usbHidReportDescriptor[39] = { /* USB report descriptor */
0x05, 0x0c, // USAGE_PAGE (Consumer Devices)
0x09, 0x01, // USAGE (Consumer Control)
0xa1, 0x01, // COLLECTION (Application)
// -------------------- common global items
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x25, 0x01, // LOGICAL_MAXIMUM (1)
0x75, 0x01, // REPORT_SIZE (1) - each field occupies 1 bit
// -------------------- misc bits
0x95, 0x05, // REPORT_COUNT (5)
0x09, 0xb5, // USAGE (Scan Next Track)
0x09, 0xb6, // USAGE (Scan Previous Track)
0x09, 0xb7, // USAGE (Stop)
0x09, 0xcd, // USAGE (Play/Pause)
0x09, 0xe2, // USAGE (Mute)
0x81, 0x06, // INPUT (Data,Var,Rel) - relative inputs
// -------------------- volume up/down bits
0x95, 0x02, // REPORT_COUNT (2)
0x09, 0xe9, // USAGE (Volume Up)
0x09, 0xea, // USAGE (Volume Down)
0x81, 0x02, // INPUT (Data,Var,Abs) - absolute inputs
// -------------------- padding bit
0x95, 0x01, // REPORT_COUNT (1)
0x81, 0x01, // INPUT (Cnst,Ary,Abs)
0xc0 // END_COLLECTION
};
Tsuneo
2016-09-29 6:26 AM
Ah I remember,
Volume up/down usages are RTC (Re-Trigger Control) type. To up/down volume stepwise, your device should send two contiguous reports, the first report holds 1 at volume up/down bit field - user presses volume up or down key the second report keeps 0 - user releases above key If your device would send just the first 1 report without the second 0, the OS could interpret this behavior as ''volume up key is continuously pressed.'' And then, it should maximize the volume. Please take care, so that it wouldn't break your PC speaker (or your ears ;) Tsuneo2016-10-01 5:25 AM
Thank you so much!
It worked :)