cancel
Showing results for 
Search instead for 
Did you mean: 

unable to ping ethernet connection with stm32h7

CJ007
Associate III
 
13 REPLIES 13
CJ007
Associate III

Hello @STea Yes, I have changed Ip according to my Pc. Still, it is not working.

 

CJ007
Associate III

Hello @STea Apart from IP, any other things have to be changed?

Hello @CJ007 ,

No other changes needed apart from IP and Netmask settings, and this is working as I mentioned before so I propose you use some traffic sniffing tool like Wireshark on you PC to look for ARP packets sent from the board and to make sure that it is visible in your network.

Make sure your PC is not using some firewall to block some responses. what I can assure you of is that your ping should work with the example I've send you, so it is either a problem with your hardware or your testing environment.

Regards 

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
CJ007
Associate III

Hello @STea  It is working with the ping code . Thanks for the zip