2025-02-13 06:50 AM - last edited on 2025-02-13 07:57 AM by SofLit
I'm using an STM32G071G8U6TR and a CP2102N-Axx-xQFN28 to communicate over USB. I am managing to get messages onto the STM32 but it seems that the first few characters of the message are coming through jumbled,
#include "main.h"
#include "UART_Polling.h"
#include "stdbool.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */
static uint16_t Buffercmp(uint8_t* pBuffer1, uint8_t* pBuffer2, uint16_t BufferLength);
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint32_t cycle;
/*********************** 0 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 *************/
uint8_t tx_buff[] = {65, 66, 67, 68, 69, 70, 71, 72, 73, 74}; //Transmitter Buffer
uint8_t true_buff[] = {77, 101, 115, 115, 97, 103, 101, 32, 114, 101, 99, 101, 105, 118, 101, 100, 10, 13}; //True buffer - 18 Characters long
uint8_t false_buff[] = {78, 111, 32, 109, 101, 115, 115, 97, 103, 101, 10, 13}; //False buffer - 12 Characters long
uint8_t v_set_buff[] = {86, 97, 108, 117, 101, 32, 115, 101, 116, 32, 65, 51, 51, 46, 52, 10, 13}; //Value Set buffer - 17 characters long
uint8_t i_set_buff[] = {73, 110, 99, 114, 101, 109, 101, 110, 116, 32, 115, 101, 116, 32, 51, 51, 46, 52, 10, 13}; //Increment Set buffer - 20 Character long
uint8_t idn_buff[] = {"FLANN MICROWAVE"};
uint8_t status_ref[] = {48, 48, 48, 48, 48, 48, 48, 48, 10, 13}; //Status bit - 10 characters long
uint8_t comm_error[] = {"UNKNOWN COMMAND"};
uint8_t rx_buff[30] = {"##############################"};
uint8_t process_buff[30] = {"##############################"};
uint8_t i=0;
uint8_t temp = 0;
bool uart_received = false;
bool query;
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_GPIO_WritePin(debug_LED_GPIO_Port, debug_LED_Pin, GPIO_PIN_SET);
HAL_UART_Receive_IT(&huart2, rx_buff, 10);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
//PollingInit();
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
if (rx_buff[0] != 0x23)
{
while(i<30)
{
if (rx_buff[i] == 0x3F) // If ?
{
tx_buff[0] = 0x74; //t
tx_buff[1] = 0x65; //e
tx_buff[2] = 0x73; //s
tx_buff[3] = 0x74; //t
tx_buff[4] = 0x20; //' '
tx_buff[5] = 0x72; //r
tx_buff[6] = 0x65; //e
tx_buff[7] = 0x63; //c
tx_buff[8] = 0x65; //e
tx_buff[9] = 0x69; //i
tx_buff[10] = 0x76; //v
tx_buff[11] = 0x65; //e
tx_buff[12] = 0x64; //d
tx_buff[13] = 0x0A;
tx_buff[14] = 0x0D;
HAL_UART_Transmit_IT(&huart2, tx_buff, 15);
}
if (rx_buff[i] > 96)
{
process_buff[i] = rx_buff[i] - 32;
rx_buff[i] = 0x23;
}
else
{
process_buff[i] = rx_buff[i];
rx_buff[i] = 0x23;
}
if (process_buff[i] == 0x3F)
{
query = true;
HAL_GPIO_TogglePin(debug_LED_GPIO_Port, debug_LED_Pin);
}
HAL_Delay(100);
i++;
}
process_buff[28] = 0x0A;
process_buff[29] = 0x0D;
HAL_UART_Transmit_IT(&huart2, process_buff, 30);
tx_buff[i] = 10;
i++;
tx_buff[i] = 13;
//HAL_UART_Transmit_IT(&huart2, tx_buff, 15);
HAL_Delay(1000);
i = 0;
while (i < 30)
{
rx_buff[i] = 0x23;
i++;
}
}
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief USART2 Initialization Function
* None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(debug_LED_GPIO_Port, debug_LED_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : debug_LED_Pin */
GPIO_InitStruct.Pin = debug_LED_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(debug_LED_GPIO_Port, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/**
* @brief Compares two buffers.
* pBuffer1, pBuffer2: buffers to be compared.
* BufferLength: buffer's length
* @retval 0 : pBuffer1 identical to pBuffer2
* >0 : pBuffer1 differs from pBuffer2
*/
static uint16_t Buffercmp(uint8_t* pBuffer1, uint8_t* pBuffer2, uint16_t BufferLength)
{
while (BufferLength--)
{
if ((*pBuffer1) != *pBuffer2)
{
return BufferLength;
}
pBuffer1++;
pBuffer2++;
}
return 0;
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
uart_received = true; /*Set Message Received varible*/
HAL_UART_Receive_IT(&huart2, rx_buff, 30); /*Load the message into the rx buffer*/
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
This is the code I am currently using. At the moment once it receives a message it's meant to scan through and check for a '?', if it does see this it responds with 'test received' and then loads the received buffer into another buffer before sending that back. When I use PuTTY to send messages I get these responses.
The message sent is CL_VALUE_SET? I get a good response for the first message, the second time I send a message I don't get any response and the third time it doesn't see the ? it seems.
2025-02-13 07:52 AM
Hello @GTann.1
Please refer to the example Projects/STM32G081B-EVAL/Examples/UART/UART_HyperTerminal_DMA to implement your application.
2025-02-13 08:04 AM - edited 2025-02-13 08:05 AM
Doesn't seem to be any synchronization between reception and processing.
The call-back is waiting for a lot of characters, and not entirely consistent from first to second. Doesn't clear the buffer, and doesn't really know how much valid data has been received.
Things that need to be volatile, and not.
Might I suggest starting with collecting singular characters, and using a circular buffering scheme, where you can determine the amount of data available to work with.