UART blocking transmition/reception and HAL driver: would need some clarification :)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-12-05 09:14 AM
Hi guys,
I'm fairly new to the world of STM32 and embedded C, and i've been playing with a STM32F401 recently.
I'm using the HAL UART driver to set a serial communication with my computer through the port COM3, and I have a few questions :
1. It took me a good while before transmitting data correctly. I believe my configuration was good but for some reason, the terminal was displaying only the fist character from my chain. I managed to sort it out by inserting a 1ms delay in the HAL_UART_Transmit driver,each time we have receive one byte. I assume it's not necessary since it wasn't in the original driver but would anyone have an idea of what is hapenning, and what i misunderstand ?
2. When trying to receive data using HAL_UART_Receive, I manage to reveive data byte by byte, but if I entry more than one character (so a chain), the function return only the first character and then go to timeout. I have a feeling there is some timing issue there but I'd like to understand what I am doing wrong and what I misunderstand.
I can add code if you think there is value, but I'd say it's more a theoretical issue.
Also, i'm now gonna look at implementing this with interupt since I beleive it will be more adequate.
Thanks a lot,
Yves
#uart #hal_uart_transmit #hal_uart_receive #hal-uart- Labels:
-
STM32Cube MCU Packages
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-12-06 12:43 AM
I managed to sort it out by inserting a 1ms delay in the HAL_UART_Transmit driver,each time we have receive one byte.
This is a sub-optimal solution, to say the least.
I suspect you manage your reception in a synchronous, blocking manner. The Cube generator spits out some framework, but you need to think about proper mechanism (algorithm) before, especially when asynchronous events like serial transmission is involved.
I can add code if you think there is value, but I'd say it's more a theoretical issue.
Presenting the code will definitely be of value.
I do not use Cube/HAL, and I don't comment on it, but there are several others here.
Also, i'm now gonna look at implementing this with interupt since I beleive it will be more adequate.
Yes, definitely.
AFAIK, Cube generates a callback function for your code, so you don't need to touch the interrupt handler itself.
Be aware interrupt priorities and runtime issues - take care to spend as few as possible time in the interrupt context, else you will block other interrupts, including follow-ups of the same interrupt.