2020-11-16 4:53 AM
In the code I wrote, it is very straightforward being initialising USART2, receiving a character from a serial monitor and turning on/off an LED based on the character received. The LED does not turn on, in this case when I type the letter 'y' on putty or any other terminal.
With this being said, if I write a simple echo program using USART2 to receive a character from the terminal and send the same character back it works. So i'm not sure why when i'm trying to receive a char without transmitting anything it doesn't work.
#include "stm32f303xe.h"
void USART2_Init(void);
void GPIO_LED_Init(void);
char USART_Read(void);
int main ()
{
//int ch = 0;
USART2_Init();
GPIO_LED_Init();
while (1)
{
//ch = USART_Read();
if (USART_Read() == 'y')
GPIOA->BSRR = (1 << 5);
else
{
//GPIOA->ODR ^= (1 << 5);
GPIOA->BSRR = (1 << 21);
for (int i=0; i<5000; i++);
}
}
}
void USART2_Init(void)
{
// Enable USART 2
RCC->APB1ENR |= (1 << 17);
// Turn on Port A clock for USART pins PA2 (TX) and PA3 (RX)
RCC->AHBENR |= (1 << 17);
// Set PA2 (TX) and PA3 (RX) as Alternate Functions
GPIOA->MODER |= (0x2 << 6) | (0x2 << 4);
// Conifgure Alternate Function Register for PA2 and PA3
GPIOA->AFR[0] |= (0x7 << 12) | (0x7 << 8);
USART2->BRR = 0x341; // Set baud rate to 9600 (8Mhz/9600)
USART2->CR1 |= (1 << 2); // Enable reciever
USART2->CR1 |= (1 << 0); // Enable USART2
}
void GPIO_LED_Init(void)
{
// Turn on clock for GPIO A (LED is connected to PA5)
//RCC->AHBENR |= (1 << 17);
// configure PA5 to General Purpose Output Mode
GPIOA->MODER |= (~(1 << 11)) | (1 << 10);
}
char USART_Read(void)
{
while (!(USART2->ISR & (1 << 5))){} // Check to see if recieve data register is empty
return USART2->RDR; // Load TX data register with ch
}
2021-03-30 12:49 PM
I believe USART2 is connected to the debugger. None of mine work either which seems weird they would use that port for the debugging and put it as the UART for the Arduino Shield.