cancel
Showing results for 
Search instead for 
Did you mean: 

Trying to setup DMA2D with TouchGFX and an FMC connected Display

BWKidd
Senior

Hi Everyone,

It was recently recommended to me that I enable DMA2D on my project to possibly alleviate another problem that I'm having detailed here (Weird horizontal artifacts in touchGFX buttons - STMicroelectronics Community). My question is, how do I properly set it up? I've read several documents on the DMA2D including How to use Chrom-ART Accelerator to refresh an LCD-TFT display on STM32 MCUs - Application note and 8. Hardware acceleration | TouchGFX Documentation but I'm left scratching my head.

If I simple enable DMA2D in MX with my current project without making any code changes like this :

BWKidd_1-1736358736097.png

 

BWKidd_0-1736358707426.png

Then I get weird distortions on some of my text:

BWKidd_2-1736358967525.png

I'm also confused as to how I should be changing my code to take full advantage of the DMA2D. In My Mind, my flushFrameBuffer function which looks like this right now

 

void TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect)
{
uint16_t* frameBuffer = getTFTFrameBuffer();
setLCDwindow(rect.x, rect.y, rect.width, rect.height);
LCD_IO_WriteReg(RAMWR);
int32_t YxWIDTH;
for (int32_t y = rect.y; y < rect.bottom(); y++) {
YxWIDTH = y * TFT_WIDTH;
for (int32_t x = rect.x; x < rect.right(); x++) {
LCD_IO_WriteData(frameBuffer[YxWIDTH + x]);
}
}

TouchGFXGeneratedHAL::flushFrameBuffer(rect);
}

Should be re-written to be something more like

void TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect)

{

uint16_t* frameBuffer = getTFTFrameBuffer();

setLCDwindow(rect.x, rect.y, rect.width, rect.height);

LCD_IO_WriteReg(RAMWR);




uint16_t* frameBuffer = getTFTFrameBuffer();

    uint16_t* destAddress = (uint16_t*)(LCD_BASE_ADDRESS + (rect.y * TFT_WIDTH + rect.x) * 2);




    // Calculate the output offset

    uint32_t OutputOffset = TFT_WIDTH - rect.width;




    // Configure DMA2D transfer

    hdma2d.Init.Mode = DMA2D_M2M;

    hdma2d.Init.ColorMode = DMA2D_OUTPUT_RGB565;

    hdma2d.Init.OutputOffset = OutputOffset;




    if (HAL_DMA2D_Init(&hdma2d) != HAL_OK) {

        // Handle error

        return;

    }




    // Start DMA2D transfer

    if (HAL_DMA2D_Start(&hdma2d,

                        (uint32_t)(frameBuffer + rect.y * TFT_WIDTH + rect.x), // Source

                        (uint32_t)destAddress, // Destination

                        rect.width,           // Width

                        rect.height)          // Height

        != HAL_OK) {

        // Handle error

        return;

    }




    // Wait for transfer to complete

    HAL_DMA2D_PollForTransfer(&hdma2d, HAL_MAX_DELAY);




    TouchGFXGeneratedHAL::flushFrameBuffer(rect);

}
 
But this doesn't display anything and I'm not even sure if I'm on the right track with this. I need help!

 

 

 

1 REPLY 1
BWKidd
Senior

Two additional observations:

1. The character distortion appears to go away when I shrink the font down to about 60 (currently its at 80)

2. If I set the option 'Use DMA2D Accelerator (Chrom-Art)' within the touchGFX settings in MX to 'No' but leave everything else the same (including leaving DMA2D enabled), the problem also goes away, though I suppose this is not surprising.