2022-01-19 9:18 AM
I am working on NUCLEO-U575ZI-Q. The code is generated with STM32CubeMX (using STM32CubeIDE) and the application uses ThreadX, which was added to the project using CubeMX.
When a thread call any function that would lead to a suspension of the thread, the function _get_ipsr() (file Middlewares\ST\threadx\ports\cortex_m33\gnu\inc\tx_port.h) is called and it directly triggers a Hard_Fault.
The error would trigger 100% of the time with some source code, and never with some other source code.
I am having this error for a while. I thought I found the solution before, but I was wrong and it was all just luck.
According to this link:
How to debug a HardFault on an ARM Cortex-M MCU | Interrupt (memfault.com)
There is a usage fault with the flag "UNALIGNED" raised. However please note that last time I had trouble with _get_ipsr(), the only flag set to 1 was in the "reserved" field of the usage fault register.
I still working on the issue but I am having trouble finding a solution. Do you have an idea on what could go wrong or how to solve this issue?
Solved! Go to Solution.
2022-01-20 6:13 AM
So I simplified the threads again and again to make them as close as possible as the examples, until I realized :
Although the execution of the function _get_ipsr() generates a crash, it is NOT responsible for the crash ; I was being very naive with the debugger.
The crash actually happens in an other thread, _get_ipsr() is just the last function called from a thread yielding, and leads to an other thread being run.
I found the source of the crash, could understand and solve the issue.
Thank you for the help.
Regards
2022-01-20 1:55 AM
Hi @Bastien LS,
Are you using the Trust Zone feature or not?
Did you try the ThreadX application provided within the STM32Cube_FW U5, does the issue appear with any of them?
regards
Haithem.
2022-01-20 4:07 AM
Hi @Haithem Rahmani
I am not using the Trust Zone feature.
I just tried 3 example applications "TX_Thread_Creation", "TX_Thread_MsgQueue", "TX_Thread_Sync" and all of them worked well.
2022-01-20 5:07 AM
@Bastien LS
then could you check what is the difference between your project and the working ones?
regards
Haithem.
2022-01-20 6:13 AM
So I simplified the threads again and again to make them as close as possible as the examples, until I realized :
Although the execution of the function _get_ipsr() generates a crash, it is NOT responsible for the crash ; I was being very naive with the debugger.
The crash actually happens in an other thread, _get_ipsr() is just the last function called from a thread yielding, and leads to an other thread being run.
I found the source of the crash, could understand and solve the issue.
Thank you for the help.
Regards
2023-10-19 3:58 PM - edited 2023-10-19 4:08 PM
@Bastien LS Did you find the solution? I may be having exactly the same problem on STM32U5A9, no trust - hard faults with UFSR=16 (unaligned), HFSR=0x400000000 (bit 30 set - forced). I cannot find any clear pattern to that. It is not a large code, plenty of SRAM, crash happens inside tx_* functions, e.g. tx_mutex_put(). When I step through it usually does not crash. I start to pull my hair out. MS has a newer version than than the one distributed by CubeMX. It seems it has some fixes.
2023-10-19 4:27 PM
I just found the problem. TX_APP_STACK_SIZE was simply too small.