2024-09-21 3:31 AM - edited 2024-09-23 12:33 AM
Hello,
I have STM32F767ZI and STM32F429ZI Nucleo board, which I want to configure in TCP Client mode. I have attached .ioc file and tcpclient.c and ethernetif.c files. This files I have downloaded from internet. Now here is my problem when I try to run this code my board is not getting connected to server. For server I am using Hercules software. My board/s are getting from ping response, but not getting connected to server.
void tcp_echoclient_connect(void)
{
ip_addr_t DestIPaddr;
/* create new tcp pcb */
echoclient_pcb = tcp_new();
if (echoclient_pcb != NULL)
{
IP4_ADDR( &DestIPaddr, DEST_IP_ADDR0, DEST_IP_ADDR1, DEST_IP_ADDR2, DEST_IP_ADDR3 );
/* connect to destination address/port */
tcp_connect(echoclient_pcb,&DestIPaddr,DEST_PORT,tcp_echoclient_connected);
}
}
/**
* @brief Function called when TCP connection established
* tpcb: pointer on the connection contol block
* err: when connection correctly established err should be ERR_OK
* @retval err_t: returned error
*/
static err_t tcp_echoclient_connected(void *arg, struct tcp_pcb *tpcb, err_t err)
{
struct echoclient *es = NULL;
if (err == ERR_OK)
{
/* allocate structure es to maintain tcp connection informations */
es = (struct echoclient *)mem_malloc(sizeof(struct echoclient));
if (es != NULL)
{
es->state = ES_CONNECTED;
es->pcb = tpcb;
sprintf((char*)data, "sending tcp client message %d", (int)message_count++);
/* allocate pbuf */
es->p_tx = pbuf_alloc(PBUF_TRANSPORT, strlen((char*)data) , PBUF_POOL);
if (es->p_tx)
{
/* copy data to pbuf */
pbuf_take(es->p_tx, (char*)data, strlen((char*)data));
/* pass newly allocated es structure as argument to tpcb */
tcp_arg(tpcb, es);
/* initialize LwIP tcp_recv callback function */
tcp_recv(tpcb, tcp_echoclient_recv);
/* initialize LwIP tcp_sent callback function */
tcp_sent(tpcb, tcp_echoclient_sent);
/* initialize LwIP tcp_poll callback function */
tcp_poll(tpcb, tcp_echoclient_poll, 1);
/* send data */
tcp_echoclient_send(tpcb,es);
return ERR_OK;
}
}
else
{
/* close connection */
tcp_echoclient_connection_close(tpcb, es);
/* return memory allocation error */
return ERR_MEM;
}
}
else
{
/* close connection */
tcp_echoclient_connection_close(tpcb, es);
}
return err;
}
My code never enters tcp_echoclient_connected(). I am stuck on this from last few days and very little information is available.
I am not using FreeRTOS.
Can you please tell me what am I doing wrong?
Any help would be appreciated.
Solved! Go to Solution.
2024-10-05 4:52 AM
So I have solved this issue. I modified my .ioc file; Firstly I enabled FreeRTOS. I also enabled Raw API from Lwip configurations.
I also had to switch to Cube IDE from IAR (don't know for what reason, but the same code is not working in IAR Environment).
2024-09-21 7:08 AM
The ethernetif.c code attached shows a MII interface not the RMII, which the Nucleo has. Its also showing the DP83848_PHY_ADDRESS, but the nucleo has a LAN8742. Try looking in the HAL example/CubeMX code for a better offering.
(The HAL examples have something that is nearly what you are trying to do - that will be a good start point into which to add your stuff)
Also double checked the memory configuration.
Take a look at
"How to create a project for STM32H7 with Ethernet and LwIP stack working" by
Cheers
Mark
2024-09-23 12:35 AM - edited 2024-09-23 12:35 AM
Sorry, I have attached wrong file for ethernetif.c. I have updated post with right file.
2024-10-05 4:52 AM
So I have solved this issue. I modified my .ioc file; Firstly I enabled FreeRTOS. I also enabled Raw API from Lwip configurations.
I also had to switch to Cube IDE from IAR (don't know for what reason, but the same code is not working in IAR Environment).