2023-01-06 3:43 PM
Hello,
I want to transmit data between two boards using TCP. To do this, one will run a client and the other will run a server. Both of these implementations follow the provided examples. The server works fine, I can connect to it from Hercules and transfer data.
The client implementation is causing me problems, as it can't seem to establish a connection to a TCP server. I can however ping it just fine. Both boards are assigned an IP via DHCP, but the address is always the same and matches with what I expect. Here is the code:
static void tcpecho_client_thread(void const *arg)
{
struct netconn *xNetConn = NULL;
err_t bind_err, connect_err;
char* b_data = "OK"; // Data to be sent
uint16_t b_len = sizeof ( b_data );
IP4_ADDR(&local_ip, IP_ADDR0_CLIENT, IP_ADDR1_CLIENT, IP_ADDR2_CLIENT, IP_ADDR3_CLIENT);
IP4_ADDR(&pc_ip, IP_ADDR0_PC, IP_ADDR0_PC, IP_ADDR2_PC, IP_ADDR3_PC);
xNetConn = netconn_new ( NETCONN_TCP );
if (xNetConn != NULL){
bind_err = netconn_bind ( xNetConn, &local_ip, TCP_PORT_NETCONN );
if(bind_err == ERR_OK){
// Try to connect to server
for(;;){
connect_err = netconn_connect ( xNetConn, &pc_ip, TCP_PORT_NETCONN);
if (connect_err == ERR_OK){
// We are connected
while(1){
BSP_LED_On(LED1);
netconn_write(xNetConn, b_data, b_len, NETCONN_COPY);
vTaskDelay(1000); // To see the result easily in Comm Operator
}
}
}
}else{
// Failed to bind the connection
BSP_LED_On(LED3);
}
}else{
// Failed to allocate a new connection
BSP_LED_On(LED3);
}
}
As I can ping it, I don't think something is fundamentally wrong. Is there something I am missing here? In the for loop, it should try to establish a connection until it succeeds, but it never actually manages to connect to something.
2023-01-06 4:20 PM
Is the server a Windows PC? Firewall enabled?
2023-01-06 4:29 PM
I have tried with the server on my Windows PC using Hercules. In that there should be at least the default Windows Firewall (at least to my knowledge).
I have also tried running a simple server on a second board. In that case, both are in the same subnet so the Firewall shouldn't play a role in that case.
2023-01-06 8:34 PM
Well, then it's the time for wireshark.
2023-01-07 3:37 AM
With Wireshark I can see the responses to my pings, but I can't see anything indicating that the board is trying to connect my PC. Should there also be a package with that information or is that just not something I can see?
2023-01-07 3:37 AM
With Wireshark I can see the responses to my pings, but I can't see anything indicating that the board is trying to connect my PC. Should there also be a package with that information or is that just not something I can see?