cancel
Showing results for 
Search instead for 
Did you mean: 

SVD error in STM32G431

hijax_pl
Associate II

Interrupts not in proper peripherals:

- WWDG is placed in I2C2,

- TIM8_CC is in peripheral TIM1,

- LPTIM1 is in LPUART1,

- USB_HP,  USB_HPLP  & USBWakeUP are in EXTI,

- CRS is in the EXTI as well.

 

1 REPLY 1
KDJEM.1
ST Employee

Hello @hijax_pl,

 

Thank you for bringing this issue to our attention.

I reported this issue internally.

Thank you for your contribution to the community.

Internal ticket number: 197834 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.