cancel
Showing results for 
Search instead for 
Did you mean: 

STMCubeF0 v1.2.1 and CMSIS Drivers question

aturowski9
Associate
Posted on April 17, 2015 at 13:06

Hi all,

I've just downloaded STM32Cube_FW_F0_V1.2.0 and applied latest patched to upgrade is to V1.2.1. I was expecting it to be fully CMSIS compliant, so for example I could use CMSIS compliant USART interface. So I went to \Drivers\CMSIS folder in STMCube and according to README.txt file there, I should find ''Driver'' folder containing CMSIS compliant drivers. Unfortunately there is no ''Driver'' folder at all. Also ''Pack'' folder is missing. Can you tell me where can I find CMSIS compliant device drivers in STM32Cube v1.2.1 please?

Kind regards,

Adam

#stm32cube #cmsis
1 REPLY 1
stst9193
Associate II
Posted on April 20, 2015 at 08:12

I do not have F0 version but F4, so it may be a bit different.  Go to /Drivers/STM32Fxxx_HAL_Driver .

Gerard