2019-06-21 6:44 AM
I try to set up an USB CDC project for a STM32L412KB Nucleo32 board using CubeIDE.
I activated the USB connection and the USB middleware with the default USB CDC setup.
If I run this code, it ends in the hardfault handler with INVSTATE raised during the USB_EnableGlobalInt(hpcd) call (HAL_PCD_Start() at stm32l4xx_hal_pcd.c:1,014 0x8000d26).
The next items on the call stacks are: <signal handler called>() at 0xfffffff9, 0x0, <signal handler called>() at 0xfffffff1 and finally HardFault_Handler() at stm32l4xx_it.c:88 0x800432a.
Currently I ran out of ideas on what to do. USB CDC worked in projects set up for the STM32F072 and F103 - should we change from the L4 to another MCU?
2019-07-20 3:03 PM
(picture courtesy of @SToma )
2019-07-21 2:43 PM
hi all.
thanks for the hint Jan, but when I do singel step, it works fine until I push resume.
So I can single step trough the whole thing and it is fine, but when I let the processor run freely again it ends up in HardFault.
So I am not any wiser from that unfortunately.
I have really been trying to figure this out, and solve how to implement clive's HardFault data.
What I can not figure out is how to make the compiler/MCU the added HardFualt addition in startup.s
Because I use Truestudio the code sample for the assembly code did not work,
So I found a example on https://nathan.vertile.com/blog/2016/05/04/stm32-hardfault-debugging/
/**
* My code in startup_stm32l412xx.s
*
*/
.section .text.Reset_Handler
.weak HardFault_Handler
.type HardFault_Handler, %function
HardFault_Handler:
movs r0,#4
movs r1, lr
tst r0, r1
beq _MSP
mrs r0, psp
b _HALT
_MSP:
mrs r0, msp
_HALT:
ldr r1,[r0,#20]
b hard_fault_handler_c
bkpt #0
.size HardFault_Handler, .-HardFault_Handler// My code in stm32l4xx_it.c
void hard_fault_handler_c(unsigned long *hardfault_args)
{
volatile unsigned long stacked_r0 ;
volatile unsigned long stacked_r1 ;
volatile unsigned long stacked_r2 ;
volatile unsigned long stacked_r3 ;
volatile unsigned long stacked_r12 ;
volatile unsigned long stacked_lr ;
volatile unsigned long stacked_pc ;
volatile unsigned long stacked_psr ;
volatile unsigned long _CFSR ;
volatile unsigned long _HFSR ;
volatile unsigned long _DFSR ;
volatile unsigned long _AFSR ;
volatile unsigned long _BFAR ;
volatile unsigned long _MMAR ;
stacked_r0 = ((unsigned long)hardfault_args[0]) ;
stacked_r1 = ((unsigned long)hardfault_args[1]) ;
stacked_r2 = ((unsigned long)hardfault_args[2]) ;
stacked_r3 = ((unsigned long)hardfault_args[3]) ;
stacked_r12 = ((unsigned long)hardfault_args[4]) ;
stacked_lr = ((unsigned long)hardfault_args[5]) ;
stacked_pc = ((unsigned long)hardfault_args[6]) ;
stacked_psr = ((unsigned long)hardfault_args[7]) ;
// Configurable Fault Status Register
// Consists of MMSR, BFSR and UFSR
_CFSR = (*((volatile unsigned long *)(0xE000ED28))) ;
// Hard Fault Status Register
_HFSR = (*((volatile unsigned long *)(0xE000ED2C))) ;
// Debug Fault Status Register
_DFSR = (*((volatile unsigned long *)(0xE000ED30))) ;
// Auxiliary Fault Status Register
_AFSR = (*((volatile unsigned long *)(0xE000ED3C))) ;
// Read the Fault Address Registers. These may not contain valid values.
// Check BFARVALID/MMARVALID to see if they are valid values
// MemManage Fault Address Register
_MMAR = (*((volatile unsigned long *)(0xE000ED34))) ;
// Bus Fault Address Register
_BFAR = (*((volatile unsigned long *)(0xE000ED38))) ;
__asm("BKPT #0\n") ; // Break into the debugger
}but this do not work, ??
what I found in Truestudio was the problem window.
It reports an hard fault and gives some info, unfortunately I do not understand what it means.
The wired thing is, I downloaded the tryout of Crossworks and it works with the board if I create an MDK-ARM V5 project in CubeMX and import it into crossworks and just run. It works. So there is no problem with the MCU or the board.
:see_no_evil_monkey:
2019-07-21 3:00 PM
Remove the WEAK settings in startup.s and comment out whatever is currently in stm32fxyz_it.c ?
I think I've posted GNU/GCC syntax code previously, blindly this should suffice..
..
TST lr, #4 /* Determine correct stack */
ITE EQ
MRSEQ R0, MSP /* Read MSP (Main) */
MRSNE R0, PSP /* Read PSP (Process) */
MOV R1, R4 /* Registers R4-R6 */
MOV R2, R5
MOV R3, R6 /* sourcer32@gmail.com */
B hard_fault_handler_c
2019-07-21 4:19 PM
> thanks for the hint Jan, but when I do singel step, it works fine until I push resume.
> So I can single step trough the whole thing and it is fine, but when I let the processor run freely again it ends up in HardFault.
My guess is, that the problem occurs in the USB interrupt service routine (ISR), and you have disabled interrupts during single-step (that's a common setting, otherwise it would be hard to single-step most practical programs).
You may perhaps want to place a breakpoint into the USB ISR and single-step from there to see, where that will take you.
Do you have a PC connected to the USB when the problem occurs?
JW
2019-07-21 5:26 PM
Should check for malloc()/free() idiocy that they like to do in interrupt context
2019-07-22 1:01 AM
Yes. For me the reason was a forgotten ISR definition in the Startup/startup_stm32l412kbux.s file. It should contain:
.word 0
.word COMP_IRQHandler
.word LPTIM1_IRQHandler
.word LPTIM2_IRQHandler
.word USB_IRQHandler
.word DMA2_Channel6_IRQHandler
.word DMA2_Channel7_IRQHandler
2019-07-22 2:54 AM
YESSSSS.
ruediger1.561124119260664E12 Hade the right answer to my problem.
Missing IRQ routine linkage .
@RKnoe Thanks
ruediger1.561124119260664E12
(Community Member)
2 hours ago
Yes. For me the reason was a forgotten ISR definition in the Startup/startup_stm32l412kbux.s file. It should contain:
.word 0
.word COMP_IRQHandler
.word LPTIM1_IRQHandler
.word LPTIM2_IRQHandler
.word USB_IRQHandler
.word DMA2_Channel6_IRQHandler
.word DMA2_Channel7_IRQHandler
2019-07-22 6:30 AM
The USB_IRQHandler vector is present in both arm and iar version of startup code, absent only in the gcc version. IMO it's a bug. @Imen DAHMEN can you please have a look? Thanks.
JW
2019-08-15 1:47 AM
Hello All,
This issue is raised internally for fix.
Thanks for your contribution.
Best Regards,
Imen
2020-01-09 10:24 AM
Note to self, Cortex-M0(+) startup.s code for Keil
HardFault_Handler\
PROC
EXPORT HardFault_Handler
EXTERN hard_fault_handler_c
MOV R1, LR
LDR R0, =hard_fault_handler_c
MOV LR, R0
MOVS R0, #4 ; Determine correct stack
TST R0, R1
MRS R0, MSP ; Read MSP (Main)
BEQ .+6 ; BEQ 2, MRS R0,PSP 4
MRS R0, PSP ; Read PSP (Process)
MOV R1, R4 ; Registers R4-R6, as parameters 2-4 of the function called
MOV R2, R5
MOV R3, R6 ; sourcer32@gmail.com
BX LR
ENDP