cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 JTAG + interrupt => Break at address "0x1fff2d58" outside of program code + overcurrent

mich35
Associate III

Hello,

I am using a sTM32L430 with a JTAG access throgh ST LINK V2 and STM32CubeIDE. The project has a few GPIO to debug and an USART to generate interrupts:

mich35_0-1699882454696.png

 

To try to undersand my problem I build a small project with STM32CubeMX to have code genrated by STM and not by me.

I added a few code to remove data from the USART BX buffer and to toggle debug pins.

 

 

void USART3_IRQHandler(void)
{
  /* USER CODE BEGIN USART3_IRQn 0 */
  int val;

  /* USER CODE END USART3_IRQn 0 */
  /* USER CODE BEGIN USART3_IRQn 1 */
    LL_GPIO_TogglePin(GPIOH, LL_GPIO_PIN_0);
	val = LL_USART_ReceiveData8(USART3);        //read byte to clear RXNE flag
    val++;
  /* USER CODE END USART3_IRQn 1 */
}
int main(void)
{
  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SYSCFG);
  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR);

  /* System interrupt init*/
  NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);

  /* SysTick_IRQn interrupt configuration */
  NVIC_SetPriority(SysTick_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),15, 0));

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART3_UART_Init();
  /* USER CODE BEGIN 2 */

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
        __delay_cycles(1000000);
        LL_GPIO_TogglePin(GPIOH, LL_GPIO_PIN_1);  // Green led
    }
  /* USER CODE END 3 */
}

 

 

I load and run the program. If an interrupt occurs during debugging I have the following issue:

Program stops (led do not toggles) and current consumption increases from 2mA to 14mA. If I click on the suspend button I have the following message:

Break at address "0x1fff3f36" with no debug information available, or outside of program code.

This address is inside the System memory.

When I have interrupts while not in debugging mode there is no issue at all.

Do you have any suggestion for this issue which prevents me of debugging capabilities?

Best regards

Mich

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
mich35
Associate III

It seems to be linked to a solder issue around the LSE quartz.

The microC reacts differently when started from JTAG or from power on...

View solution in original post

3 REPLIES 3
AScha.3
Chief II

boot0 pin (PH3 ?) needs pulldown. or gnd . otherwise jumping to system bootloader mode...

If you feel a post has answered your question, please click "Accept as Solution".

PH3 has a pull-down

mich35
Associate III

It seems to be linked to a solder issue around the LSE quartz.

The microC reacts differently when started from JTAG or from power on...