STM32H750 DMA ADC crush
- 2 replies
- 2380 views
Hello,
I'm using STM32H750VBT
When I'm trying to use DMA for ADC data collection I'm experiencing MCU crush. Currently I know that issue happens when DMA fill half of defined buffer.
I'm using STM32CubeIDE and builded in CubeMX. To precize issue I used debug By SWD STLink. to be able run code step by step I desabled continuous conversion mode. Attaching my Cube MX ADC settings:


And DMA settings

After pre configured by CubeMX initiation I'm calling conversion by
HAL_ADC_Start_DMA(&hadc2, (uint32_t*)testDMA, 20);
And entering into while (1) loop where calling adc2 conversion
HAL_ADC_Start(&hadc2);
after every loop I checking testDMA[] buffer
and DMA cycle by cycle fills testDMA as well up to [8], but on testDMA[9] debugger shows errors and don't able to cintinue code running (example on attached screen)

I tried to change in HAL_ADC_Start_DMA(&hadc2, (uint32_t*)testDMA, 20); from 20 to any another value and issue happens on half of the defined buffer. array testDMA is big enough, in that case it's uint16_t testDMA [60];
Probably isue occurs because MCU can't call/execute interrupt



void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc)
I'm attaching full project. My cubeIDE version is 1.14.1
Please help me run my DMA which would fill my buffer fully and would run succesfully interrupt
void HAL_ADC_ConvCpltCallback