2020-12-30 12:10 AM
Hello!
I got a new STM32 Nucleo-H723ZG, now i am testing about many days, but i have a big Problem, is use the new Stm32CubeIDE 1.5.2 with actually Firmware for the MCU.
The Problem is, i loaded a new Cube Project with Default Values, for the Board without any Changes, now when i run or debug my project, hangs my MCU on this Code:
HAL_ETH_Init:
/* Ethernet Software reset */
/* Set the SWR bit: resets all MAC subsystem internal registers and logic */
/* After reset all the registers holds their respective reset values */
SET_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR);
/* Get tick */
tickstart = HAL_GetTick();
/* Wait for software reset */
while (READ_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR) > 0U)
{
if(((HAL_GetTick() - tickstart ) > ETH_SWRESET_TIMEOUT))
{
/* Set Error Code */
heth->ErrorCode = HAL_ETH_ERROR_TIMEOUT;
/* Set State as Error */
heth->gState = HAL_ETH_STATE_ERROR;
/* Return Error */
return HAL_ERROR;
}
}
i got an HAL_ERROR, and the MCU Goes to from the Main Function to the Error_Handler...
What is the Problem? This code is generated from the MxCube and its unchanged...
Thanks,
Daniel
2020-12-30 2:15 AM
Please try an example from Cube package for your board: this or others:
(If you have downloaded Cube H7 package to your machine, it is already on your machine).
These examples are known to work much better than Cube generated code.
-- pa
2021-01-20 11:17 PM
Hi Pavel,
Just directly build and upload the firmware? NO other changes required?
Please suggest.
Thanks and Regards,
JM
2021-11-17 5:09 AM
Hello all,
I'm running into the same trouble than explain above by Sany.
To be more precise I do have a bunch of hardware and some of them are not working due to this issue while the other part is running properly.
Does someone solve it ? Many thanks
Edit: I'm running an STM32H750 chip
2021-11-17 5:30 AM
Hi,
This may not be the answer, but I had a problem with H743 DMA from uart and it turned out to be something really simple:
Regeneration with the .ioc places these in the wrong order:
MX_GPIO_Init();
MX_DMA_Init();
MX_USART3_UART_Init();
Correct order shown above.
Hope this helps someone!!
Chris
2021-11-17 3:38 PM
STM32H750's closest relatives are STM32H753 and 743.
Look for examples for boards with these chips.
2023-01-05 10:13 PM
check phy clk or rst
2023-07-03 12:48 AM
Hi DFell.1
Have you solved this problem yet?
I'm using Stm322h750 with custom board, and when active the ETH RMII, program runs into Error_Handler() and all other functions not working.