cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 LPTIM compare mode

catalin78
Visitor

Hi, I use STM32CubeMX 6.10.0 and I have a STM32H7 CPU.

The LPTIM is a frequency counter that can give an ISR when the

counter reached a specified value; after reaching this value it starts

again from zero (ARR mode), or it continues towards the max value

on 16 bits and then starts again from zero (CMP mode)

My question is: can I configure from CubeMX this LPTIM in CMP mode?

To me it seems there is no settings for this, whatever I do it's still in ARR mode ..

the solution would be to make manual code changes ?

 

0 REPLIES 0