cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 SPI DMA transfer performance problems

TheImmortal
Associate III

I cant get faster SPI performance, in every SPI DMA request mcu receiving 164 bytes of data, the maximum request rate what I got is about 1KHz, total number of bytes is only ~ 164 * 1000 = 164KB, I need to reach 8KHz rate, MCU and other clocks is set to almost maximum values, on STM32H7 MCU with many other tasks I reached without any problems 12KHz rate, with N6 I cant get event near of required transfer speed in any configurations, If I rising request rate I getting SPI busy error, where can be the problem ? What peripherals or other settings is responsible for SPI transfer and interfere there ? I can attach .IOC file or more info.
In my setup SPI requests is controlled by HAL_TIM_PeriodElapsedCallback(), sometimes I need to stop requests in case when synchronization is lost, timer fires function for next SPI DMA transfer and in case of error (in my case I getting SPI busy error) the timer for request is stopped, timer fires simple function:
void nextPacket(){
    if (HAL_SPI_Receive_DMA(&hspi5, buff, 164) != HAL_OK) { 
        HAL_TIM_Base_Stop_IT(&htim16);
        printf("Spi E\n");
    }
}

There is no difference if I choosing GPDMA1 or HPDMA1, the transfer rate does not reaching more, same is for SPI frequency.

DMA settings:

TheImmortal_0-1750933721125.png

TheImmortal_2-1750933814756.png

 

SPI settings:

TheImmortal_1-1750933759715.png

 

2 REPLIES 2
TDK
Super User

Show your code and show why you think the max request rate is 1 kHz. Almost certainly a code bug here. Consider not calling printf in code you want to be fast.

If you feel a post has answered your question, please click "Accept as Solution".

Printf fires just in case when there is spi error, for tests in SPI callback I commented out everything except LED toggle, with oscilloscope I checked led toggle freq to confirm, I miscalculated before, real frequency is 2x because there is used toggle, and I checked more what I can get, I reached ~4kHz, in my code there just simple functions for test:

void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef * hspi){
    if (hspi->Instance == SPI5) HAL_GPIO_TogglePin(GPIOP, GPIO_PIN_7);
}

void nextIRpacket(){
    if (HAL_SPI_Receive_DMA(&hspi5, buff, 164) != HAL_OK){
        HAL_TIM_Base_Stop_IT(&htim16);
        printf("Spi E\n");
    }
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef* htim) {
    if (htim == &htim16){
        if (Resync == 0) {
            __HAL_TIM_SET_COUNTER(&htim16, 0);
            nextPacket();
            HAL_GPIO_TogglePin(GPIOP, GPIO_PIN_6);
        }
    }
}
 
Just while ago I found how to overcome this problem, I increased SPI speed to 20MHz, I got 8kHz rate, now 164byte transaction takes ~63us, then pause ~47us, if SPI freq. is 12.5MHz then there is about 10us pause and its not enough, I dont know the reason why SPI is busy for such long time after transaction, something in SPI lower level code or hw consumes to much time, with STM32H7 I dont had any issues there, down to ~11MHz SPI freq.