cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H573: ETH SWRESET fails, ETH_DMAMR_SWR stays set, timeout

Lionheart1810
Associate II

I want to initialize the STM32H573 ETH module using the STM32CubeMX code generator (see ioc file attached). It should run in MII mode using an external transceiver.

I kept the configuration unchanged, however it always jumps to ErrorHandler, because HAL_ETH_Init returns HAL_ERROR on timeout of ETH_DMAMR_SWR at the following routine:

  SET_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR);

  /* Get tick */
  tickstart = HAL_GetTick();

  /* Wait for software reset */
  while (READ_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR) > 0U)
  {
    if (((HAL_GetTick() - tickstart) > ETH_SWRESET_TIMEOUT))
    {
      /* Set Error Code */
      heth->ErrorCode = HAL_ETH_ERROR_TIMEOUT;
      /* Set State as Error */
      heth->gState = HAL_ETH_STATE_ERROR;
      /* Return Error */
      return HAL_ERROR;
    }
  }

From what I've read on this forum, the ETH somehow needs an external clock input from the transceiver. However, ETH_REF_CLK is only defined in RMII mode, but I want MII mode with RX and TX clocks. Does it still need permanently running clock? ETH_RX_CLK is currently served from the transceiver with 2.5 MHz (in 10 Mbps mode), the ETH module itself is clocked 100 MHz from PLL1Q:

Screenshot_20250203_191600.png

I even tried rising the timeout threshold, but even 50 s is failing. Any ideas on how to get the initialization through?

1 ACCEPTED SOLUTION

Accepted Solutions
Lionheart1810
Associate II

Figured out the error. I was missing the propagation of the reset signal to the external PHY for bootstrap configuration. Just added it to the HAL_ETH_MspInit.

View solution in original post

8 REPLIES 8
alister
Lead

ETH_REF_CLK is for RMII. ETH_RX_CLK and ETH_TX_CLK are for MII.

I observed HAL_ETH_Init failing similarly for the STM32H7S78-DK last year and posted that and a fix at https://community.st.com/t5/stm32cubemx-mcus/bugs-caveats-misc-fixes-stm32h7s-cube/td-p/710992. For clarity, the peripheral clock's fix in HAL_ETH_MspInit was:

 

 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ETH1REF;
 PeriphClkInit.Eth1RefClockSelection = RCC_ETH1REFCLKSOURCE_PHY;

 

 

Lionheart1810
Associate II

This section does not exist in the autogenerated HAL_ETH_MspInit:

Spoiler
void HAL_ETH_MspInit(ETH_HandleTypeDef* heth)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
  if(heth->Instance==ETH)
  {
  /* USER CODE BEGIN ETH_MspInit 0 */

  /* USER CODE END ETH_MspInit 0 */
    /* Peripheral clock enable */
    __HAL_RCC_ETH_CLK_ENABLE();
    __HAL_RCC_ETHTX_CLK_ENABLE();
    __HAL_RCC_ETHRX_CLK_ENABLE();

    __HAL_RCC_GPIOB_CLK_ENABLE();
    __HAL_RCC_GPIOG_CLK_ENABLE();
    __HAL_RCC_GPIOC_CLK_ENABLE();
    __HAL_RCC_GPIOH_CLK_ENABLE();
    __HAL_RCC_GPIOA_CLK_ENABLE();
    /**ETH GPIO Configuration
    PB8     ------> ETH_TXD3
    PG14     ------> ETH_TXD1
    PG13     ------> ETH_TXD0
    PG11     ------> ETH_TX_EN
    PC1     ------> ETH_MDC
    PC2     ------> ETH_TXD2
    PC3     ------> ETH_TX_CLK
    PH6     ------> ETH_RXD2
    PA1     ------> ETH_RX_CLK
    PA0     ------> ETH_CRS
    PC4     ------> ETH_RXD0
    PH7     ------> ETH_RXD3
    PA2     ------> ETH_MDIO
    PC5     ------> ETH_RXD1
    PA3     ------> ETH_COL
    PA7     ------> ETH_RX_DV
    */

    GPIO_InitStruct.Pin = GPIO_PIN_8;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF11_ETH;
    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_14|GPIO_PIN_13|GPIO_PIN_11;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF11_ETH;
    HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4
                          |GPIO_PIN_5;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF11_ETH;
    HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF11_ETH;
    HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);

    GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_0|GPIO_PIN_2|GPIO_PIN_3
                          |GPIO_PIN_7;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
    GPIO_InitStruct.Alternate = GPIO_AF11_ETH;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  /* USER CODE BEGIN ETH_MspInit 1 */

  /* USER CODE END ETH_MspInit 1 */

  }

}

Also, there is no RCC_PERIPHCLK_ETH... (as it is most likely directly clocked from PLL1Q).

Anything I am missing?

My bad, my clock fix applies the STM32H7S/R, not the STM32H7!

I've not used newer than Cube v5.5 with an STM32H7... Check your Cube generated code for the following macros. The __HAL_RCC_GPIOx macros are only necessary for the GPIO ports that have pins connected/used.

    __HAL_RCC_ETH1MAC_CLK_ENABLE();
    __HAL_RCC_ETH1TX_CLK_ENABLE();
    __HAL_RCC_ETH1RX_CLK_ENABLE();
  
    __HAL_RCC_GPIOC_CLK_ENABLE();
    __HAL_RCC_GPIOA_CLK_ENABLE();
    __HAL_RCC_GPIOB_CLK_ENABLE();

 

Check other resources:

The code you mention isn't included in your Cube-generated HAL_ETH_MspInit looks very familiar. You need all of that.

Please post whether it's an ST dev board and which one, or a custom board, your Cube version, and if it's an ST dev board, whether you loaded the board's default config in Cube.

@STea, could you or a colleague assist Lionheart1810 please?

Lionheart1810
Associate II

I am using STM32H573, not STM32H7 series.

STM32CubeMX version: 6.13.0
Firmware package version: STM32Cube FW_H5 V1.4.0

It is a custom board. I use DP83826 as Ethernet transceiver and 25 MHz oscillator. However, afaik it should be independent of the transceiver in MII mode for the reset.

I tried figuring it out and adding the missing code myself, but there are no such RCC_PERIPHCLK_ETH... macros in the entire HAL. I also just tried to initialize a blank project with just ETH enabled without success.

PHY is the clock source for both Rx and Tx in MII mode.

So, you need the TX_CLK and RX_CLK outputs from PHY to be connected to ETH_TX_CLK and ETH_RX_CLK pins (marked in DS as ETH_MII_TX_CLK=PC3 and ETH_MII_RX_CLK=PA1) of the 'H5 respectively. These pins have to be set to AF in GPIOx_MODER and to the proper AF number (11) in GPIOx_AFR[]. Besides, RCC_AHB1ENR.ETHEN, .ETHTXEN, .ETHRXEN must be set (all 3 bits).

Read the RCC and ETH chapters in Reference Manual.

If CubeMX/Cube/HAL does not work for you, well, just don't use it, and program through registers directly.

PHY of course must be strapped (or configured through SMI) to MII mode.

JW

Lionheart1810
Associate II

Figured out the error. I was missing the propagation of the reset signal to the external PHY for bootstrap configuration. Just added it to the HAL_ETH_MspInit.