2020-06-07 4:07 AM
Hi All,
I am looking at the HRTIM CBC example here:
The questions are centred around EE5 and EE8 external inputs.
I have 2 questions, that probably someone can clear my understanding.
(1) EE8 is available only with PB8, but PB8 s used for the Boot configuration (P88 is pulled down via a resistor to boot from Flash)How is the situation handled ?
(2) As per the resource manual, I understand that EE5 is not associated with a filter and is thus considered a Fast channel.
Around line#246:
LL_HRTIM_EE_SetSrc(HRTIM1, LL_HRTIM_EVENT_5, LL_HRTIM_EEV5SRC_GPIO);
LL_HRTIM_EE_SetPolarity(HRTIM1, LL_HRTIM_EVENT_5, LL_HRTIM_EE_POLARITY_HIGH);
LL_HRTIM_EE_SetSensitivity(HRTIM1, LL_HRTIM_EVENT_5, LL_HRTIM_EE_SENSITIVITY_LEVEL);
LL_HRTIM_EE_SetFastMode(HRTIM1, LL_HRTIM_EVENT_5, LL_HRTIM_EE_FASTMODE_DISABLE);As a result, the Fast mode option appears to be disabled.
Around line#250:
LL_HRTIM_EE_SetSrc(HRTIM1, LL_HRTIM_EVENT_8, LL_HRTIM_EEV8SRC_GPIO);
LL_HRTIM_EE_SetPolarity(HRTIM1, LL_HRTIM_EVENT_8, LL_HRTIM_EE_POLARITY_HIGH);
LL_HRTIM_EE_SetSensitivity(HRTIM1, LL_HRTIM_EVENT_8, LL_HRTIM_EE_SENSITIVITY_BOTHEDGES);
LL_HRTIM_EE_SetFilter(HRTIM1, LL_HRTIM_EVENT_8, LL_HRTIM_EE_FILTER_NONE)EEV8 Filter appears to be disabled, but at line#282 the EEV8 Filter seems to applied:
LL_HRTIM_TIM_SetCaptureTrig(HRTIM1, LL_HRTIM_TIMER_D, LL_HRTIM_CAPTUREUNIT_1, LL_HRTIM_CAPTURETRIG_EEV_8);
LL_HRTIM_TIM_SetCaptureTrig(HRTIM1, LL_HRTIM_TIMER_D, LL_HRTIM_CAPTUREUNIT_2, LL_HRTIM_CAPTURETRIG_EEV_8);
LL_HRTIM_TIM_SetEventFilter(HRTIM1, LL_HRTIM_TIMER_D, LL_HRTIM_EVENT_8, LL_HRTIM_EEFLTR_BLANKINGCMP1);Question 2a) :Why is the Filter disabled and then enabled later ?
Now, both events are used to Reset the output waveform at Line#288
LL_HRTIM_OUT_SetOutputResetSrc(HRTIM1, LL_HRTIM_OUTPUT_TD1, LL_HRTIM_OUTPUTRESET_TIMCMP3|LL_HRTIM_OUTPUTRESET_EEV_5
|LL_HRTIM_OUTPUTRESET_EEV_8);Question 2b):
Both External events (pins PB8 & PB9) are tied together; PB5 is Level triggered while PB8 is edge triggered. Both of them are used to Reset the Output PWM. What is the need to use both EEV5 and EE8. I am trying to understand the methodology in there.
Can someone bring n a bit of clarification ?
Thanks,
Manu
2020-06-08 11:05 AM
Any thoughts/suggestions ?
Thanks,
Manu