2022-12-06 1:35 PM
I'm designing a board G4 MCU and want to be able to power the board from USB C as well as debug or program the board.
I tried using this post as reference to get a better understanding.
https://community.st.com/s/feed/0D53W000007zVncSAE
Solved! Go to Solution.
2022-12-07 6:06 AM
Hello if you need more information on USBPD vs STM32 please check wiki articles.
There is also various helpful examples:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-06 8:34 PM
It's not realistic to debug via a direct USB interface to the board. The workable approach is to use SWD and put a header on the board to interface with a programmer such as the STLINK-V3MINI. No need for a separate chip. Note that the board needs powered elsewhere as the programmer does not provide power.
You can't power the MCU directly from USB as the voltage is too high. You will need an LDO to take the ~5V USB supply down to something like 3.3V which is usable by the MCU. You can use the 5V supplied by the USB for whatever else is on your board, so long as you stay within the power budget.
2022-12-07 1:46 AM
What is the purpose of USB C power delivery if the MCU is not capable of handling the voltages? it's the interface connected directly to the MCU pins? How would i manage the voltages from USB if they are supplied directly to the MCU?
2022-12-07 5:05 AM
Why don't you read some documents on USBPD and the solutions provided by ST? There is a choice of X-Nucleo extension boards for PD experiments and a bunch of examples and step-by-step tutorials on this topic - easy to find on ST website. Just read, listen, look at the schematics.
2022-12-07 6:06 AM
Hello if you need more information on USBPD vs STM32 please check wiki articles.
There is also various helpful examples:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-07 7:02 AM
The purpose is to provide power.
These are electronics 101 questions. Managing voltages is a fairly common theme. Google linear regulators.
2022-12-08 3:56 AM
Sorry. Maybe my question wasn't very clear. The board is designed to control several frequency synthesizers, up/down converters, filters, switches, and amplifiers. I want the MCU to both control these devices and be able to supply voltage via usb if there is no standard supply. I was asking more so how the voltage supply from USB is distributed. I'll read more on the subject. Thanks.