2022-08-22 07:54 AM
Please Share, suggest suitable library or sample codes for Mounting SD card as Mass Storage with Virtual COM port option.
Thanks
Solved! Go to Solution.
2022-08-25 08:10 AM
Hello @SLoga.2 and welcome to the Community :)
The application available under STM32CubeG0 MCU package, may help you to use the USB device application based on the Mass Storage Class (MSC):
STM32Cube_FW_G0_V1.6.0\Projects\STM32G0C1E-EV\Applications\USB_Device\MSC_Standalone
You can follow the instructions on the readme files.
When your question is answered, please close this topic by choosing Select as Best.
Imen
2022-08-25 08:10 AM
Hello @SLoga.2 and welcome to the Community :)
The application available under STM32CubeG0 MCU package, may help you to use the USB device application based on the Mass Storage Class (MSC):
STM32Cube_FW_G0_V1.6.0\Projects\STM32G0C1E-EV\Applications\USB_Device\MSC_Standalone
You can follow the instructions on the readme files.
When your question is answered, please close this topic by choosing Select as Best.
Imen
2022-08-25 06:58 PM
Thanks Imen,
Working
2022-08-26 02:53 AM
Glad to know the issue has been solved.
Please allow me to close this thread and thank you for your contribution.