2020-12-03 9:30 AM - last edited on 2024-07-03 3:23 AM by Andrew Neil
Hey,
I am using a STM32F7676vit6 Controller an try to set up a SAI connection to my audio CODEC now my problem is that the CODEC has two Serial outputs and one serial input. So i configured:
SAI1A to be the transmitting master SAI1B is a synchronous Slave which is configured to be in sync with SAI1A. SAI2B is also configured a synchronous Slave and configured to be in sync with SAI1A. I also use DMA on all three channels.
Now i receive data on SAI1B and but not on SAI2B (SAI1A works fine). Only wired thing is that after txCpltCallback the SCK and FS do not stop....
I really don't know what to try anymore please help ;).
I use CubeIDE my sai.c file looks like:
/* Includes ------------------------------------------------------------------*/ #include "sai.h" #include "gpio.h" #include "dma.h" /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ SAI_HandleTypeDef hsai_BlockA1; SAI_HandleTypeDef hsai_BlockB1; SAI_HandleTypeDef hsai_BlockB2; DMA_HandleTypeDef hdma_sai1_a; DMA_HandleTypeDef hdma_sai1_b; DMA_HandleTypeDef hdma_sai2_b; /* SAI1 init function */ void MX_SAI1_Init(void) { hsai_BlockA1.Instance = SAI1_Block_A; hsai_BlockA1.Init.AudioMode = SAI_MODEMASTER_TX; hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS; hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE; hsai_BlockA1.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE; hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY; hsai_BlockA1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_192K; hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE; hsai_BlockA1.Init.MonoStereoMode = SAI_STEREOMODE; hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING; hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED; if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_LSBJUSTIFIED, SAI_PROTOCOL_DATASIZE_32BIT, 2) != HAL_OK) { Error_Handler(); } hsai_BlockB1.Instance = SAI1_Block_B; hsai_BlockB1.Init.AudioMode = SAI_MODESLAVE_RX; hsai_BlockB1.Init.Synchro = SAI_SYNCHRONOUS; hsai_BlockB1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE; hsai_BlockB1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY; hsai_BlockB1.Init.SynchroExt = SAI_SYNCEXT_DISABLE; hsai_BlockB1.Init.MonoStereoMode = SAI_STEREOMODE; hsai_BlockB1.Init.CompandingMode = SAI_NOCOMPANDING; hsai_BlockB1.Init.TriState = SAI_OUTPUT_NOTRELEASED; if (HAL_SAI_InitProtocol(&hsai_BlockB1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_32BIT, 2) != HAL_OK) { Error_Handler(); } } /* SAI2 init function */ void MX_SAI2_Init(void) { hsai_BlockB2.Instance = SAI2_Block_B; hsai_BlockB2.Init.AudioMode = SAI_MODESLAVE_RX; hsai_BlockB2.Init.Synchro = SAI_SYNCHRONOUS_EXT_SAI1; hsai_BlockB2.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE; hsai_BlockB2.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY; hsai_BlockB2.Init.MonoStereoMode = SAI_STEREOMODE; hsai_BlockB2.Init.CompandingMode = SAI_NOCOMPANDING; hsai_BlockB2.Init.TriState = SAI_OUTPUT_NOTRELEASED; if (HAL_SAI_InitProtocol(&hsai_BlockB2, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_32BIT, 2) != HAL_OK) { Error_Handler(); } } static uint32_t SAI1_client =0; static uint32_t SAI2_client =0; void HAL_SAI_MspInit(SAI_HandleTypeDef* hsai) { GPIO_InitTypeDef GPIO_InitStruct; /* SAI1 */ if(hsai->Instance==SAI1_Block_A) { /* SAI1 clock enable */ if (SAI1_client == 0) { __HAL_RCC_SAI1_CLK_ENABLE(); } SAI1_client ++; /**SAI1_A_Block_A GPIO Configuration PE4 ------> SAI1_FS_A PE5 ------> SAI1_SCK_A PE6 ------> SAI1_SD_A */ GPIO_InitStruct.Pin = SAI1A_FS_Pin|SAI1A_SCK_Pin|SAI1A_DAC_SDATA_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF6_SAI1; HAL_GPIO_Init(GPIOE, &GPIO_InitStruct); /* Peripheral DMA init*/ hdma_sai1_a.Instance = DMA2_Stream1; hdma_sai1_a.Init.Channel = DMA_CHANNEL_0; hdma_sai1_a.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_sai1_a.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sai1_a.Init.MemInc = DMA_MINC_ENABLE; hdma_sai1_a.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_sai1_a.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_sai1_a.Init.Mode = DMA_NORMAL; hdma_sai1_a.Init.Priority = DMA_PRIORITY_LOW; hdma_sai1_a.Init.FIFOMode = DMA_FIFOMODE_DISABLE; if (HAL_DMA_Init(&hdma_sai1_a) != HAL_OK) { Error_Handler(); } /* Several peripheral DMA handle pointers point to the same DMA handle. Be aware that there is only one stream to perform all the requested DMAs. */ __HAL_LINKDMA(hsai,hdmarx,hdma_sai1_a); __HAL_LINKDMA(hsai,hdmatx,hdma_sai1_a); } if(hsai->Instance==SAI1_Block_B) { /* SAI1 clock enable */ if (SAI1_client == 0) { __HAL_RCC_SAI1_CLK_ENABLE(); } SAI1_client ++; /**SAI1_B_Block_B GPIO Configuration PE3 ------> SAI1_SD_B */ GPIO_InitStruct.Pin = GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF6_SAI1; HAL_GPIO_Init(GPIOE, &GPIO_InitStruct); /* Peripheral DMA init*/ hdma_sai1_b.Instance = DMA2_Stream5; hdma_sai1_b.Init.Channel = DMA_CHANNEL_0; hdma_sai1_b.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_sai1_b.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sai1_b.Init.MemInc = DMA_MINC_ENABLE; hdma_sai1_b.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_sai1_b.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_sai1_b.Init.Mode = DMA_NORMAL; hdma_sai1_b.Init.Priority = DMA_PRIORITY_LOW; hdma_sai1_b.Init.FIFOMode = DMA_FIFOMODE_DISABLE; if (HAL_DMA_Init(&hdma_sai1_b) != HAL_OK) { Error_Handler(); } /* Several peripheral DMA handle pointers point to the same DMA handle. Be aware that there is only one stream to perform all the requested DMAs. */ __HAL_LINKDMA(hsai,hdmarx,hdma_sai1_b); __HAL_LINKDMA(hsai,hdmatx,hdma_sai1_b); } /* SAI2 */ if(hsai->Instance==SAI2_Block_B) { /* SAI2 clock enable */ if (SAI2_client == 0) { __HAL_RCC_SAI2_CLK_ENABLE(); } SAI2_client ++; /**SAI2_B_Block_B GPIO Configuration PA0/WKUP ------> SAI2_SD_B */ GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF10_SAI2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* Peripheral DMA init*/ hdma_sai2_b.Instance = DMA2_Stream6; hdma_sai2_b.Init.Channel = DMA_CHANNEL_3; hdma_sai2_b.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_sai2_b.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sai2_b.Init.MemInc = DMA_MINC_ENABLE; hdma_sai2_b.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_sai2_b.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_sai2_b.Init.Mode = DMA_NORMAL; hdma_sai2_b.Init.Priority = DMA_PRIORITY_LOW; hdma_sai2_b.Init.FIFOMode = DMA_FIFOMODE_DISABLE; if (HAL_DMA_Init(&hdma_sai2_b) != HAL_OK) { Error_Handler(); } /* Several peripheral DMA handle pointers point to the same DMA handle. Be aware that there is only one stream to perform all the requested DMAs. */ __HAL_LINKDMA(hsai,hdmarx,hdma_sai2_b); __HAL_LINKDMA(hsai,hdmatx,hdma_sai2_b); } } void HAL_SAI_MspDeInit(SAI_HandleTypeDef* hsai) { /* SAI1 */ if(hsai->Instance==SAI1_Block_A) { SAI1_client --; if (SAI1_client == 0) { /* Peripheral clock disable */ __HAL_RCC_SAI1_CLK_DISABLE(); } /**SAI1_A_Block_A GPIO Configuration PE4 ------> SAI1_FS_A PE5 ------> SAI1_SCK_A PE6 ------> SAI1_SD_A */ HAL_GPIO_DeInit(GPIOE, SAI1A_FS_Pin|SAI1A_SCK_Pin|SAI1A_DAC_SDATA_Pin); HAL_DMA_DeInit(hsai->hdmarx); HAL_DMA_DeInit(hsai->hdmatx); } if(hsai->Instance==SAI1_Block_B) { SAI1_client --; if (SAI1_client == 0) { /* Peripheral clock disable */ __HAL_RCC_SAI1_CLK_DISABLE(); } /**SAI1_B_Block_B GPIO Configuration PE3 ------> SAI1_SD_B */ HAL_GPIO_DeInit(GPIOE, GPIO_PIN_3); HAL_DMA_DeInit(hsai->hdmarx); HAL_DMA_DeInit(hsai->hdmatx); } /* SAI2 */ if(hsai->Instance==SAI2_Block_B) { SAI2_client --; if (SAI2_client == 0) { /* Peripheral clock disable */ __HAL_RCC_SAI2_CLK_DISABLE(); } /**SAI2_B_Block_B GPIO Configuration PA0/WKUP ------> SAI2_SD_B */ HAL_GPIO_DeInit(GPIOA, GPIO_PIN_0); HAL_DMA_DeInit(hsai->hdmarx); HAL_DMA_DeInit(hsai->hdmatx); } }
To make sure that every thing works in sync i first start both receiving Block and than the Transmitting one like:
HAL_SAI_Receive_DMA(&hsai_BlockB1, (uint8_t*) &meas->BufferADC23[0], BufferSize); //ADC 01 HAL_SAI_Receive_DMA(&hsai_BlockB2, (uint8_t*) &meas->BufferADC01[0], BufferSize); //ADC 23 HAL_SAI_Transmit_DMA(&hsai_BlockA1, (uint8_t*) &LookupTable[0], LookupTableSize); //DAC 01
I am very grateful for any help
Solved! Go to Solution.
2020-12-04 3:43 AM
Hey,
I have found the root cause i think:
It seams that even if I configure the "External Synchro Out" Signal in the STM32CubeIDE that the init function, does not care about it.
Remains unchanged! To me that looks clearly like a bug from the STM32CubeIDE.
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
/* SAI1 init function */
void MX_SAI1_Init(void)
{
hsai_BlockA1.Instance = SAI1_Block_A;
hsai_BlockA1.Init.AudioMode = SAI_MODEMASTER_TX;
hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS;
hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockA1.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE;
hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY;
hsai_BlockA1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_192K;
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockA1.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED;
if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_LSBJUSTIFIED, SAI_PROTOCOL_DATASIZE_32BIT, 2) != HAL_OK)
{
Error_Handler();
}
hsai_BlockB1.Instance = SAI1_Block_B;
hsai_BlockB1.Init.AudioMode = SAI_MODESLAVE_RX;
hsai_BlockB1.Init.Synchro = SAI_SYNCHRONOUS;
hsai_BlockB1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockB1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY;
hsai_BlockB1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockB1.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockB1.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockB1.Init.TriState = SAI_OUTPUT_NOTRELEASED;
if (HAL_SAI_InitProtocol(&hsai_BlockB1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_32BIT, 2) != HAL_OK)
{
Error_Handler();
}
To fix that and enable the first block SAI1 to output the external sync signal, it is necessary to manually configure both sub-Blocks of the SAI1:
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_OUTBLOCKA_ENABLE;
hsai_BlockB1.Init.SynchroExt = SAI_SYNCEXT_OUTBLOCKA_ENABLE;
I hope that i can help others which might run into similar problems.
Cheers,
Luca
2020-12-04 3:43 AM
Hey,
I have found the root cause i think:
It seams that even if I configure the "External Synchro Out" Signal in the STM32CubeIDE that the init function, does not care about it.
Remains unchanged! To me that looks clearly like a bug from the STM32CubeIDE.
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
/* SAI1 init function */
void MX_SAI1_Init(void)
{
hsai_BlockA1.Instance = SAI1_Block_A;
hsai_BlockA1.Init.AudioMode = SAI_MODEMASTER_TX;
hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS;
hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockA1.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE;
hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY;
hsai_BlockA1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_192K;
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockA1.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED;
if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_LSBJUSTIFIED, SAI_PROTOCOL_DATASIZE_32BIT, 2) != HAL_OK)
{
Error_Handler();
}
hsai_BlockB1.Instance = SAI1_Block_B;
hsai_BlockB1.Init.AudioMode = SAI_MODESLAVE_RX;
hsai_BlockB1.Init.Synchro = SAI_SYNCHRONOUS;
hsai_BlockB1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockB1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY;
hsai_BlockB1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockB1.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockB1.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockB1.Init.TriState = SAI_OUTPUT_NOTRELEASED;
if (HAL_SAI_InitProtocol(&hsai_BlockB1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_32BIT, 2) != HAL_OK)
{
Error_Handler();
}
To fix that and enable the first block SAI1 to output the external sync signal, it is necessary to manually configure both sub-Blocks of the SAI1:
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_OUTBLOCKA_ENABLE;
hsai_BlockB1.Init.SynchroExt = SAI_SYNCEXT_OUTBLOCKA_ENABLE;
I hope that i can help others which might run into similar problems.
Cheers,
Luca
2024-03-22 3:35 AM - edited 2024-06-14 1:10 AM
glad that you found it!
@LFrei.2 wrote:I hope that i can help others which might run into similar problems.
The best way to do that is to Mark the Solution - then people will see that the thread is "Solved".
Also, please try to keep the title brief.
2024-06-13 10:17 PM
Hi Luca @LFrei.2
Thank you so much for posting the solution of the problem. I don't know how many days of my life would be wasted without your solution. I am writing the 4 years later and ST still has not solved the problem in CubeMX.
Thanks and wish you many happy day!
2024-07-03 6:14 AM
Hi @Duddie ,
Checking on my side using STM32CubeMX 6.11.1, I see that following lines are properly generated:
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_OUTBLOCKA_ENABLE;
hsai_BlockB1.Init.SynchroExt = SAI_SYNCEXT_OUTBLOCKA_ENABLE;
To have these lines generated, I need to:
I'm not sure that this is really an STM32CubeMX or STM32CubeIDE issue requiring fix.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.