cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32F767 Nucleo Ethernet does not always start

arainho
Associate II
Posted on September 18, 2016 at 03:00

Hi All,

I have noticed that the Stm32F767 Nucleo does not always start Ethernet reliably. For testing I used one of the example on the STM32Cube_FW_F7_V1.4.0 for the STM32F746ZG-Nucleo base of LWIP. 

I set up a DOS windows to ping the board, and from every 10 resets or power ups of the board, about half of them fail to respond to the pings.

I am evaluating the Stm32F767 and Lan8720A and I am a bit disappointed at this reliability issue.

I also wrote a small program using Keil Rtos and also have the same problem. 

The link leds are both on and the activity led blinks but no ping response.

 Looking at the Ethernet MMC register just the receive crc error register increments.

Any ideas on how to debug this?

#ethernet
20 REPLIES 20
Amel NASRI
ST Employee
Posted on October 20, 2016 at 12:55

Hello,

The Ethernet limitations are described in

http://www.st.com/content/ccc/resource/technical/document/errata_sheet/group0/23/a6/11/0b/30/24/46/a5/DM00257543/files/DM00257543.pdf/jcr:content/translations/en.DM00257543.pdf

.

Please note that a new device revision will be available to fix these limitations.

For more details, please contact your FAE or distributor.

-STM32 Forums Moderator

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.