2019-01-14 5:46 AM
Hello,
I use PA2 pin to wake up from standby mode with a STM32F765 MCU.
I am a bit confused because it is wrotten in HAL Manual (UM1905) at the page 607 : This pin is forced in input pull-down configuration and is active on rising edges.
If i let the pin not connected and whatever the choosen polarity , the mcu is waken up from standby mode without any voltage.
To get worked, I have to solder a pull down resistor at the input.
My problem is i want to be waken up with a uart frame and the default state is high state which gives consumption (1Mohm => 3.3uA).
Could you confirm my tests are ok because i did not find any information in any manual !
Thanks,