cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746 Core Halt on ETH cable Pulgin

lavanya
Associate III

I am using CUBEMX Version  6.10 

STMCUBEIDE                        1.16.0

Enabled LWIP ETH With FREERTOS

I configured on internal Timer TIM1 

as soon as I connect Eth Cable program counter not reaching threads & Timer callback / TIM6(systick update).

I checked in fault handlers it is not reaching here 

ETH State in eth handler is (READY STATE --> START STATE)

Error code in eth handler is zero.

Here I have attached my .ioc file

I have updated flash ld file as per repository code

0 REPLIES 0