2019-01-12 8:38 AM
Hello.
I'm interfacing my STM32F7 with the following current sensing chip:
https://datasheets.maximintegrated.com/en/ds/MAX34408-MAX34409.pdf
And page 8 describes that I need to send a repeated START command during communication. I cannot find a method of doing this using the I2C HAL library.
Could somebody please point me in the right direction please?
Thanks
2019-01-12 10:19 AM
Apply the following memory R/W calls which will apply the required repeat START transaction:
HAL_I2C_Mem_Write
HAL_I2C_Mem_Read
HAL_I2C_Mem_Write_IT
HAL_I2C_Mem_Read_IT
HAL_I2C_Mem_Write_DMA
HAL_I2C_Mem_Read_DMA
Also using the search engine, found the same solution here:
2019-01-16 7:18 AM
Hi @Adam Davis ,
You can use the following APIs that allow to manage repeated start condition:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.