2014-06-16 4:41 AM
Hello,
I downloaded ''STM32F4x7_ETH_LwIP_V1.1.0'' package and I want to make ''httpserver_socket'' example working with no success.I am getting hardfault ISR !I want to ask if there is somebody who succeeded to make it running.Thanks in advance for help.PS: my hardware is working fine since one of the standalone examples is working fine.Cheers #ethernet-freertos
2014-12-19 9:43 AM
Hi Bauer,
As wrote above; this package was fully tested based on the HW/SW environment listed in the release notes. I can see 2 possible root cause of your issue:2015-01-12 9:09 AM
Jasmin,
I have found the solution. There is a bug in the freeRTOS examples. The projects include FreeRTOS port for ARM Cortex M3 instead of ARM Cortex M4F.You can check that. The package includes the file whose the path:Utilities\Third_Party\FreeRTOSV7.3.0\portable\IAR\ARM_CM3Regards,