cancel
Showing results for 
Search instead for 
Did you mean: 

SPI2 not working on STM32F746BG

zin10
Associate II

I am experiencing an issue with SPI communication on the STM32F746BG microcontroller:

  • Current Setup:
    • SPI2 connected to ADC
    • SPI6 connected to Ethernet
  • Current Behavior:
    • When testing SPI2 (ADC) alone: Works properly
    • When testing SPI6 (Ethernet) alone: Works properly
    • When using both SPI2 and SPI6 together: SPI2 stops responding
    • When replacing SPI2 with SPI4: Both SPI4 and SPI6 work together properly

Question: Why does SPI2 stop responding when used simultaneously with SPI6, while SPI4 works fine in the same configuration?"

1 REPLY 1
TDK
Super User

Probably a bug in the code. Perhaps interrupts are overloading the system, or DMA is out of bandwidth, or some other issue.

If you feel a post has answered your question, please click "Accept as Solution".