STM32F427VI = Assertion "sys_timeout: timeout != NULL, pool MEMP_SYS_TIMEOUT is empty"
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-06-17 08:10 AM
Hi all,
I am using a STM32F427VI MCU.
I developed an application using LWIP library.
I am trying to run an application that I finished to develop and test in three boards.
This application works as expected in all of them. When I burn the application to a fourth board I can see that the app stopts in this function:
void HandleEthernet()
{
/* Read a received packet from the Ethernet buffers and send it
to the lwIP for handling */
ethernetif_input(&gnetif);
/* Handle timeouts */
sys_check_timeouts();
}
I got this errors in the debug console:
Assertion "sys_timeout: timeout != NULL, pool MEMP_SYS_TIMEOUT is empty" failed at line 212 in C:/Users/alex_s/STM32Cube/Repository/STM32Cube_FW_F4_V1.24.1/Middlewares/Third_Party/LwIP/src/core/timeouts.c
Assertion "pbuf_alloc: pbuf p->payload properly aligned" failed at line 297 in C:/Users/alex_s/STM32Cube/Repository/STM32Cube_FW_F4_V1.24.1/Middlewares/Third_Party/LwIP/src/core/pbuf.c
Assertion "check p->payload + p->len does not overflow pbuf" failed at line 304 in C:/Users/alex_s/STM32Cube/Repository/STM32Cube_FW_F4_V1.24.1/Middlewares/Third_Party/LwIP/src/core/pbuf.c
The problems is here. I think that somehow the application can't allocate the memory
sys_timeout(u32_t msecs, sys_timeout_handler handler, void *arg)
#endif /* LWIP_DEBUG_TIMERNAMES */
{
struct sys_timeo *timeout, *t;
u32_t now, diff;
timeout = (struct sys_timeo *)memp_malloc(MEMP_SYS_TIMEOUT);
if (timeout == NULL) {
LWIP_ASSERT("sys_timeout: timeout != NULL, pool MEMP_SYS_TIMEOUT is empty", timeout != NULL);
return;
}
LWIPOPTS.h configuration
#ifndef __LWIPOPTS__H__
#define __LWIPOPTS__H__
#include "main.h"
#ifdef __cplusplus
extern "C" {
#endif
#define LWIP_TIMEVAL_PRIVATE 0
#define SYS_LIGHTWEIGHT_PROT 0
#define NO_SYS 1
#define MEM_ALIGNMENT 4
#define MEM_SIZE (16*1024)
#define MEMP_NUM_PBUF 16
/* MEMP_NUM_UDP_PCB: the number of UDP protocol control blocks. One per active UDP "connection". */
#define MEMP_NUM_UDP_PCB 6
/* MEMP_NUM_TCP_PCB: the number of simulatenously active TCP connections. */
#define MEMP_NUM_TCP_PCB 10
/* MEMP_NUM_TCP_PCB_LISTEN: the number of listening TCP connections. */
#define MEMP_NUM_TCP_PCB_LISTEN 6
/* MEMP_NUM_TCP_SEG: the number of simultaneously queued TCP segments. */
#define MEMP_NUM_TCP_SEG TCP_SND_QUEUELEN
/* MEMP_NUM_SYS_TIMEOUT: the number of simulateously active timeouts. */
#define MEMP_NUM_SYS_TIMEOUT 11
/* ---------- Pbuf options ---------- */
/* PBUF_POOL_SIZE: the number of buffers in the pbuf pool. */
#define PBUF_POOL_SIZE 16
/* PBUF_POOL_BUFSIZE: the size of each pbuf in the pbuf pool. */
#define PBUF_POOL_BUFSIZE 2500
/* ---------- TCP options ---------- */
#define LWIP_TCP 1
#define TCP_TTL 255
/* Controls if TCP should queue segments that arrive out of
order. Define to 0 if your device is low on memory. */
#define TCP_QUEUE_OOSEQ 0
/* TCP Maximum segment size. */
#define TCP_MSS (2500 - 40) /* TCP_MSS = (Ethernet MTU - IP header size - TCP header size) */
/* TCP sender buffer space (bytes). */
#define TCP_SND_BUF (16*TCP_MSS)
/* TCP_SND_QUEUELEN: TCP sender buffer space (pbufs). This must be at least
as much as (2 * TCP_SND_BUF/TCP_MSS) for things to work. */
#define TCP_SND_QUEUELEN (8* TCP_SND_BUF/TCP_MSS)
/* TCP receive window. */
#define TCP_WND (8*TCP_MSS)
/* ---------- ICMP options ---------- */
#define LWIP_ICMP 1
/* ---------- DNS options ---------- */
#define LWIP_DNS 1
#define LWIP_DHCP 1
/* ---------- UDP options ---------- */
#define LWIP_UDP 1
#define UDP_TTL 255
/* ---------- Statistics options ---------- */
#define LWIP_STATS 0
#define LWIP_PROVIDE_ERRNO 1
#define LWIP_NETIF_LINK_CALLBACK 1
#define LWIP_NETIF_STATUS_CALLBACK 1
#if (NO_SYS==0)
#define LWIP_NETCONN 1
#else
#define LWIP_NETCONN 0
#endif
#define LWIP_SOCKET 0
#ifdef __cplusplus
}
#endif
#endif /*__LWIPOPTS__H__ */
Any idea how can I avoid this? and why this is happening only in one MCU?
- Labels:
-
Ethernet
-
STM32F4 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-01-13 02:48 AM
Default number of simultaneously active timeouts is defined in opt.h as:
#define LWIP_NUM_SYS_TIMEOUT_INTERNAL (LWIP_TCP + IP_REASSEMBLY + LWIP_ARP + (2*LWIP_DHCP) + LWIP_AUTOIP + LWIP_IGMP + LWIP_DNS + PPP_NUM_TIMEOUTS + (LWIP_IPV6 * (1 + LWIP_IPV6_REASS + LWIP_IPV6_MLD)))
For my SNTP client I ran out of available timeouts and was able to fix it adding +1 to this macro.
Why one of your MCU acts differently - sorry couldn't help you