2025-01-05 11:31 PM
Hi,
I am trying to use internal DMA configuration on STM32F415RGT6. Couldn't find the relevant support for enabling the dma and also watching off the dma transmit and receive flag as an Endpoint mode. The STM is operating as an Endpoint device. I am trying to send BULK IN. Existing doesn't have the internal DMA enabled. It is waiting for the entire Data to get transmitted. I need to use DMA for USB to perform parallel data send and resume other operations we have in our application.
2025-01-06 05:27 AM
Hi @S_Srinath
Did you make sure to consider data alignment? (by multiple of 4 packet). In fact, internal DMA doesn't allow sending data from non-word aligned addresses.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-14 08:40 PM
Hi @FBL,
We tried with 4 bytes aligned packet. We couldn't get the data from the HOST. Our DMA configuration is done on ST which acts like the Device mode. We tried checking the AHB Buss error bit also. I couldn't get any leads over it. It will be helpful if you could share any sample test codes for configuring this internal DMA.