2025-02-11 12:49 AM - last edited on 2025-02-11 2:22 AM by Andrew Neil
Hi,
I am interfacing my stm32f4 as a modbus TCP/IP client and my laptop act as server(modsim).
So i need to give me the best example for that with modbus tcp/IP communication and also provide the portable Modbus TCP/IP stack so i can easily integrate into the my code.
Thanks in advanced.
2025-02-11 2:03 AM - edited 2025-02-11 2:03 AM
Hello @MSury.1,
This link might help you: Solved: modbus tcp-ip (server/client) Over ethernet - STMicroelectronics Community
With Regards,
2025-02-17 4:27 AM
I have tried to port modbus library into the my workspace but I am not able to compiled in my stm32 workspace due to the error as comes.
https://community.st.com/t5/stm32-mcus-embedded-software/i-need-help-to-modbus-tcp-ip/td-p/582205