2012-11-06 08:55 PM
I am trying to transfer data packets from a meter ( has a usb port) using the board to my PC. I am trying to transfer real time data packets using control transfer. What would be the configurations for the mini and micro usb USBs on my board? Could you help me, please?
#connect-uart-to-pc #thanks #stm32f4-otg2012-11-07 03:58 AM
The mini USB is connected to the F103 ST-LINK device, not the F407.
You'll need a different board that natively supports two USB interfaces, or examine if you can wire up a second one if the pin use/assignments permit.2012-11-12 11:38 AM
Hey Clive,
Thanks for your Replay. I got a question. I see on STM32F4-Discovery board, two USBs. One USB Port which they call Mini USB (Connected to CN1), and the other is connected to CN5 ''on the go''. Is OTG is not a valid way of coomunication? I am kind of confused ! ________________ Attachments : stm32f4_discovery.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzSb&d=%2Fa%2F0X0000000bP1%2Fuq4VKc9CRT5WzyA3Hb9obRmdrj8yDvwRQr1foPUfg.I&asPdf=false2012-11-12 11:52 AM
As noted CN1 is useless to your application of the STM32F4 chip, it's not connected to it.
CN5 can take an A or B micro cable, so you can either connect it to a PC, or use it to connect (host) a flash drive etc. You'll need to compile and install suitable software, The USB examples mostly target the STM32x0x-EVAL boards. If you want to use both USB peripherals (host and device) on the STM32F407 chip you'll need a different board. The STM32F4-Discovery board also does not support HS USB as it does not have a PHY.2012-11-13 04:24 PM
2012-11-19 05:18 PM
Got a question,
I am getting this error codesevery timeI try to build the project. 1- 'LIBUSB_OUT_EP' undeclared here (not in a function) Line 192 2-Description Resource Path Location Type 'LIBUSB_OUT_PACKET' undeclared here (not in a function) usbd_libusb_core.cline 194 3- near intitalization for 'USB_Lib_USB_cb'' ________________ Attachments : STM32F4_Discovery_RCC.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzkV&d=%2Fa%2F0X0000000bOz%2FHAUNkYGHogcxsZotSgELP2zOCdSXFbXkYJK1rqy9E58&asPdf=false2012-11-20 12:12 AM
''You'll need a different board that natively supports two USB interfaces''
Or maybe use something like this for the connection to the PC:http://www.ftdichip.com/Products/Cables/USBTTLSerial.htm
It connects direct to the microcontroller's UART pins - be sure to choose the correct voltage version! Or this: