2015-01-17 9:54 AM
Hi,
I'm using HAL driver to configure ADC module. This is my code:void adc_config(){ AdcHandle.Instance = ADC1; __ADC1_CLK_ENABLE(); HAL_ADC_DeInit(&AdcHandle); AdcHandle.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV2; AdcHandle.Init.Resolution = ADC_RESOLUTION12b; AdcHandle.Init.DataAlign = ADC_DATAALIGN_RIGHT; AdcHandle.Init.ScanConvMode = DISABLE; AdcHandle.Init.EOCSelection = DISABLE; AdcHandle.Init.ContinuousConvMode = ENABLE; AdcHandle.Init.DMAContinuousRequests = DISABLE; AdcHandle.Init.NbrOfConversion = 1; AdcHandle.Init.DiscontinuousConvMode = DISABLE; AdcHandle.Init.NbrOfDiscConversion = 0; AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; AdcHandle.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T1_CC1; HAL_ADC_Init(&AdcHandle); ADC_ChannelConfTypeDef sConfig; sConfig.Channel = ADC_CHANNEL_10; //PC0 sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; sConfig.Offset = 0; HAL_ADC_ConfigChannel(&AdcHandle, &sConfig);}int adc_convert(){ HAL_ADC_Start(&AdcHandle);//Start the conversion HAL_ADC_PollForConversion(&AdcHandle,10);//Processing the conversion return HAL_ADC_GetValue(&AdcHandle); //Return the converted data}When I compile that, i get an error messages ''undefined reference to `HAL_ADC_DeInit'''. The error message is the same for all HAL_ADC functions... I use Eclipse + GCC.When I manually open stm32f4xx_hal_adc.c file, I can find the definition of the HAL functions.When I use CTR+Left click on the function in main.c, i get the .h file od hal_adc, but when i again click on the function i don't get the .c file of the hal_adc. What is the problem?Thanks #adc #eclipse #hal2015-01-19 8:25 AM
Hi,
File stm32f4xx_hal_adc.c has to be added into your porject tree, not only the header file so that functions can be used.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.