2015-08-27 12:41 AM
void HAL_CAN_MspInit(CAN_HandleTypeDef* hcan)
{
GPIO_InitTypeDef GPIO_InitStruct;
if(hcan->Instance==CAN)
{
/* USER CODE BEGIN CAN_MspInit 0 */
/* USER CODE END CAN_MspInit 0 */
/* Peripheral clock enable */
__CAN_CLK_ENABLE();
/**CAN GPIO Configuration
PB8 ------> CAN_RX
PB9 ------> CAN_TX
*/
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_CAN;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USER CODE BEGIN CAN_MspInit 1 */
/* USER CODE END CAN_MspInit 1 */
}
}
/* CAN init function */
void MX_CAN_Init(void)
{
hcan.Instance = CAN;
hcan.pTxMsg = &TxMessage; // Pointer initialization
hcan.pRxMsg = &RxMessage;
hcan.Init.Prescaler = 3;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SJW = CAN_SJW_1TQ;
hcan.Init.BS1 = CAN_BS1_13TQ;
hcan.Init.BS2 = CAN_BS2_2TQ;
hcan.Init.TTCM = DISABLE;
hcan.Init.ABOM = DISABLE;
hcan.Init.AWUM = DISABLE;
hcan.Init.NART = DISABLE;
hcan.Init.RFLM = DISABLE;
hcan.Init.TXFP = DISABLE;
HAL_CAN_Init(&hcan);
}
while(1) //main while
{
while(hcan.State == HAL_CAN_STATE_BUSY);
TxMessage.IDE = CAN_ID_STD;
TxMessage.StdId = 0x001;
TxMessage.ExtId = 0x001;
TxMessage.RTR = CAN_RTR_DATA; //For Remote Request CAN_RTR_REMOTE
TxMessage.DLC = 8;
TxMessage.Data[0] = 0x01;
TxMessage.Data[1] = 0x02;
TxMessage.Data[2] = 0x03;
TxMessage.Data[3] = 0x04;
TxMessage.Data[4] = 0x05;
TxMessage.Data[5] = 0x06;
TxMessage.Data[6] = 0x07;
TxMessage.Data[7] = 0x08;
HAL_CAN_Transmit(&hcan,100);
while(hcan.State == HAL_CAN_STATE_BUSY);
HAL_Delay(10);
HAL_CAN_Receive(&hcan,CAN_FIFO0,100);
while(hcan.State == HAL_CAN_STATE_BUSY);
HAL_Delay(10);
HAL_CAN_Receive(&hcan,CAN_FIFO1,100);
}
I'm running the same code in two boards.
I can see the CAN signals with oscilloscope. But the hcan.pRxMsg is always empty.
I use latest CubeMx.
Am i missing sth?
#stm32cube #can #bug #stm32-can
2015-08-27 05:11 AM
Where do you set the RX filters?
2015-08-27 09:24 AM
/* CAN init function */
void MX_CAN_Init(void)
{
hcan.Instance = CAN;
hcan.pTxMsg = &TxMessage; // Pointer initialization
hcan.pRxMsg = &RxMessage;
hcan.Init.Prescaler = 3;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SJW = CAN_SJW_1TQ;
hcan.Init.BS1 = CAN_BS1_13TQ;
hcan.Init.BS2 = CAN_BS2_2TQ;
hcan.Init.TTCM = DISABLE;
hcan.Init.ABOM = DISABLE;
hcan.Init.AWUM = DISABLE;
hcan.Init.NART = DISABLE;
hcan.Init.RFLM = DISABLE;
hcan.Init.TXFP = DISABLE;
HAL_CAN_Init(&hcan);
CAN_FilterConfTypeDef sFilterConfig;
/* Configure the CAN Filter 0 for FIFO 0 with node id */
sFilterConfig.FilterNumber = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh =0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.BankNumber = 14;
if(HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)
{
myerror = HAL_ERROR;
}
}
CubeMX should make a default filtering setup by itself!!!
I lose so many time with this little bugs since this cubemx thing..
Thank you peacock.jack... Tyvm