2019-11-08 2:39 PM
Hi. I'm using STM32CubeMX Code Generation for the STM32H745-DISCO (STM32H745XIHx chip). with firmware STM32Cube_FW_H7 V1.5.0.
When a timer is set as the timebase source for the M7 core, an assert is triggered in the call to 'HAL_NVIC_SetPriority(...)' in stm32h7xx_hal_timebase_tim.c's implementation of HAL_InitTick(...).
This is because HAL_InitTick is called with a TickPriority value of 16, which is invalid.
The default HAL implementation of HAL_InitTick sets the 'uwTickPrio' variable to its parameter 'TickPriority', while the stm32h7xx_hal_timebase_tim implementation does not. This was not a problem with previous firmwares (F7, at least) because the HAL_InitTick function was only called with TICK_INT_PRIORITY as a parameter. With the H7 implementation HAL_InitTick is inexplicably called with uwTickPrio as a parameter in HAL_RCC_ClockConfig(...). Since uwTickPrio is never set, HAL_InitTick is called with an invalid parameter.
A quick workaround is to manually set uwTickPrio to TICK_INT_PRIORITY in main.c.
Attached is a minimal example that demonstrates the problem.
2019-11-11 2:11 PM
This is strange. HAL_Init calls HAL_Init_Tick() with a constant parameter, TICK_INT_PRIORITY, which should be defined in your project's hal_conf.h
-- pa
2019-11-11 6:48 PM
Yes, it is strange. The call to HAL_Init_Tick in HAL_Init is correct. It is the generated call to HAL_Init_Tick in HAL_RCC_ClockConfig that has the issue.
2019-11-12 12:50 AM
Hello @therealergo ,
I assume this is the same issue as the one reported in https://community.st.com/s/question/0D50X0000BGvYPsSQN.
Please note that it is already tracked internally to be fixed in coming releases of STM32Cube FW packages.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-05-24 2:43 AM
Not fixed yet.
Manual fix is manually add somewhere in main()
uwTickPrio = TICK_INT_PRIORITY;
before calling SystemClock_Config();
In USER CODE BEGIN 1 or USER CODE BEGIN Init block