cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE not showing stm32c0 series - when starting new project (screenshot attached).

DalipSharma
Associate III

DalipSharma_0-1699291907180.png

 

When I am trying to create a new project for STM32C011 series microcontroller, STM32 cube IDE not showing it in microcontroller selection list.

Do i need to install support/package for STM32C0 series, to create workspace for the STM32C0 workspace.

Thanks & Regards.

1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Evangelist III

Please update CubeIDE or CubeMX to a recent version.

View solution in original post

6 REPLIES 6
Hagi
Associate II

That's strange, for me it's the first one listed. Maybe your network is blocking something when CubeIDE is updating the devices list.

Hagi_0-1699303385758.png

As for the need to install a support package, it's not really necessary at this stage of project creation. I don't have any support for F0 family and it is properly listed on the MCU selection screen.

Hagi_1-1699303642435.png

 

 



Pavel A.
Evangelist III

Please update CubeIDE or CubeMX to a recent version.

Thanks for reply. Maybe i will try to update IDE and then check the response of IDE.

Thanks for the reply. Will update it to latest version and then check it.

Even on STM32 cube MCU packages, i checked, its not listing STM32C0 series. 

DalipSharma
Associate III

Uninstalled old version and installed : en.st-stm32cubeide_1.13.2_18220_20230914_1601_x86_64.exe. 

Its working now. Thanks for the support.