STM32CubeIDE and STM32Cube FW_F1 V1.8.5 firmware Package , SWJ problem.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-07-28 5:07 AM
IDE : STM32CubeIDE Version 1.12.1
firmware Package: FW_F1 V1.8.5
Device : STM32F103C8T6
I found that when I set MX -> Pinout & Configuration -> System Core -> Sys -> Debug = No Debug, I can't use some pins, especially those associated with JTAG.
I discovered that in the file stm32f1xx_hal_msp.c the HAL_MspInit function does not put __HAL_AFIO_REMAP_SWJ_DISABLE to configure the AFIO_MAPR register (SWJ_CFG) and this register in the STM32F103C8T6 after the reset is put in Full SWJ mode (JTAG-DP + SW-DP) (information obtained from section 9.4.2 of the RM0008 manual. )
I force the code as follows:
void HAL_MspInit(void)
{
/* USER CODE BEGIN MspInit 0 */
/* USER CODE END MspInit 0 */
__HAL_RCC_AFIO_CLK_ENABLE();
__HAL_RCC_PWR_CLK_ENABLE();
/* System interrupt init*/
/* Peripheral interrupt init */
/* PVD_IRQn interrupt configuration */
HAL_NVIC_SetPriority(PVD_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(PVD_IRQn);
/* USER CODE BEGIN MspInit 1 */
#if defined(RELEASE_VERSION)
__HAL_AFIO_REMAP_SWJ_DISABLE(); // I think this line should be generated by itself if I set Debug = No Debug.
#endif
/* USER CODE END MspInit 1 */
}
With that I manage to make the pins functional as GPIO.
Solved! Go to Solution.
- Labels:
-
STM32F1 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-11-30 12:40 AM
Hi @FAndr.5 ,
Please note that reported issue should be already fixed with latest STM32CubeMX revision (6.10.0) already available on st.com.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-06 7:58 AM
Hi @FAndr.5 ,
Thanks for bringing this issue to our attention, it is reported internally and sorry for late answer.
Internal ticket number: 160875 (This is an internal tracking number and is not accessible or usable by customers).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-11-30 12:40 AM
Hi @FAndr.5 ,
Please note that reported issue should be already fixed with latest STM32CubeMX revision (6.10.0) already available on st.com.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.