2025-02-21 09:46 AM
Hi,
The STM32Cube and Azure RTOS hands-on workshop MOOC is missing the example workshop material file. The MOOC link takes one to a single PDF with setup instructions which include a link for "STM32-AZURE-RTOS-WS-Material.exe". This required file is missing from the Google Drive location.
Could you please make the workshop materials available?
1. MOOC page:
2. Google Drive link from above MOOC:
3. Workshop setup PDF with link to materials which takes one back to step (2) above:
Many thanks,
Matthew.
2025-02-21 12:46 PM
Hello @Matthew1
I will check on this with The concerned team after the weekend and I will get back to you ASAP.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.