cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cubeâ„¢ available for the new STM32L0 MCUs

Amel NASRI
ST Employee
Posted on April 30, 2014 at 18:47

Rich development ecosystem helps designers cut power consumption to the bone

 

Enhanced

http://www.st.com/stm32cube-pr3

design tools, including the Power Consumption Calculator wizard now support the STM32L0, helping designers use the new devices to reach ultra-low power-consumption targets.

http://www.st.com/stm32cube-pr3

helps accelerate generation of initialization code and simplifies porting of designs between different STM32 devices.

Some numbers

  • run consumption down

    to 87�A/MHz
  • 440nA stop mode with full RAM data retention

  • fast wakeup time of 3.5�s

      

And

  • Unique process technology that maintains stability over a wide temperature range

  • The world�s lowest power consumption at 125�C

  • The world�s lowest ADC power consumption (The 12-bit on-chip ADC draws only 48�A when operating at 100ksample/s)

Coming soon

  • A new STM32L0 Nucleo board featuring Morpho and Arduino-compatible connectors and fully supported by mbed.org (mid 2014)
  • Discovery kit that will host an ePaper display as well as a linear capacitive touch and self-test measurement system enabling users to measure MCU power consumption in real-time (mid 2014)

  • Optimized sample-code snippets dedicated to STM32L0 MCUs will also be available for both the Nucleo board and Discovery kit, providing further help for designers seeking the lowest power-consumption profile.

Finally

 

For engineers in Europe, ST is hosting a series of

 

http://www.st.com/ulpseminar

 

with a focus on RF. Attendees get a free STM32 L0 Nucleo kit and the M24SR NFC/RFID memory shield.

 

For further information and to download STM32Cube free of charge, please visit

http://www.st.com/stm32cube

.

STM32CubeL0

http://www.st.com/web/en/news/n3551

#stm32l051xx_cubelib-bug

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 REPLIES 2
lakhwinder_singh
Associate
Posted on June 13, 2014 at 09:18

Hello

I am new in ST community,i am using STM32F302BVT6 micocontroller,can I use STM32 Cube to evaluate the micocontroller and als ohow to post here,please guide

denlok
Associate II
Posted on June 07, 2015 at 14:14

STM32L051xx_CUBELIB\source\stm32l0xx_hal_gpio.c

 268:       temp &= ~((uint32_t)0x0F) << (4 * (position & 0x03));

must be

 268:       temp &= ~(((uint32_t)0x0F) << (4 * (position & 0x03)));