cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 setup with 2 x HS controllers

donpedro
Associate II
 
2 REPLIES 2
donpedro
Associate II

Hello all,

Is there a way to setup a system with 2 x USB High Speed controller easily on an STM32 controller?

As far as I can tell, even the STM32H7 only has 1 HS PHY (ULPI interface), as the other one is FS only, even though the internal controller is HS.

1) Is this limitation true, or does there exist any STM32 with 2xUSB HS ?

2) Is there a way to easily add a secondary HS controller to an STM32?

Any interface will do (SPI or similar for data):

Thanks,

/pedro

KDJEM.1
ST Employee

Hello @donpedro​,

I recommend you to use the STM32MPU1.

This device have two physical ports supported using an on-chip 2-port high-speed PHY.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.