2018-05-24 3:14 AM
Hello Community,
I am using the function HAL_UART_Transmit to send a string of 4 character in output to a display. I order to test the function first I am using a serial monitor (TERMITE) on my PC but i got this problem in the title.
I am using NUCLEO-H743ZI with HAL libraries generated with CubeMX and this is my code in the main file:
uint8_t mbuff[1];
uint8_t transBuff[4];mbuff[0]='d';transBuff[0]='c';transBuff[1]='o';transBuff[2]='s';transBuff[3]='a';HAL_UART_Transmit(&huart3, transBuff, 1, 200);
HAL_Delay(1000);printf('\n....');HAL_UART_Transmit(&huart3, (uint8_t *)mbuff, sizeof(mbuff), 200); HAL_Delay(1000); printf('\n');in the first case when i send mbuff i receive 'd' and that is correct, but when I send a string with more than one character (transBuff) instead of receiving 'cosa' i receive 'c7a'.
Has anyone got the same problem?
the configuration of USART is the following:
void MX_USART3_UART_Init(void)
{huart3.Instance = USART3;
huart3.Init.BaudRate = 115200; huart3.Init.WordLength = UART_WORDLENGTH_7B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_NONE; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16; huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart3.Init.Prescaler = UART_PRESCALER_DIV2; huart3.Init.FIFOMode = UART_FIFOMODE_DISABLE; huart3.Init.TXFIFOThreshold = UART_TXFIFO_THRESHOLD_1_8; huart3.Init.RXFIFOThreshold = UART_RXFIFO_THRESHOLD_1_8; huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart3) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
All the setting in the serial monitor are correct. Using Printf function the reception is always good but using the HAL_UART_Transmit function with more than one character there are some problems. Could be a problem with the clock syncronization? Should be better to decreas the BAUD rate in this case?
Thank you
#hal_uart_transmit #stm32cube_fw_h7_v1.0.0 #usart #nucleo-h743zi2018-05-24 5:41 AM
Hello,
your UART is configured in 7-bits word length and it is causing wrong configuration in your terminal (most probably).
huart3.Init.WordLength = UART_WORDLENGTH_7B; //Your configuration
huart3.Init.WordLength = UART_WORDLENGTH_8B; //Most probably expected on terminal side�?�?
Best regards,
Tilen