cancel
Showing results for 
Search instead for 
Did you mean: 

Running freertos on stm32F407

Eya
Associate

i can not create a simple project on stm32F407 that blink leds with the use of freertos

5 REPLIES 5
STTwo-32
ST Employee

Asslema @Eya and welcome to the ST Community.

Could you please elaborate more about your issue following those guidelines.

Liltek zina.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

i want to create a simple project that blink led on board stm32f407 , using freertos, but still can't , if you can guide throught it ,

STTwo-32
ST Employee

I think there are many tutorials that should show you how to setup such a blinking led project (such as this one that is not an official ST Tutorial). Also, there are many GitHub codes and tutorials to do that (such as this one that is not an ST official document).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

mfgkw
Senior III
Saket_Om
ST Employee

Hello @Eya 

Please refer to the example below.

STM32CubeF4/Projects/STM32446E_EVAL/Applications/FreeRTOS/FreeRTOS_ThreadCreation at master · STMicroelectronics/STM32CubeF4 · GitHub

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om