cancel
Showing results for 
Search instead for 
Did you mean: 

Resolve unexpected interrupt when using SAI to output sound

PExco.1
Associate

Hi,

I'm trying to output sound on my touchGFX application on STM32H747I-DISCO.

I used the BSP example from STM32Cube_FW_H7_v1.11 ( wich work fine) to implement the same process in a thread in my main code.

So as a first step, i expect to loop the example .bin sound of the exemple while my touchGFX app is running.

-Initialisation of the SAI through BSP_AUDIO_OUT_Init() seems to work fine and return no error.

-So i use ST-LINK utility to flash the .bin file.

My probleme is, when calling BSP_AUDIO_OUT_Play(), a noise is loop on the jack output, and the debug enter in a infinite loop due to Unexpected Interrupt, so the TouchGFX app is block.

My guess would be that i didn't register well the callback fonction of the DMA used to fill the SAI, so I tried to implement BSP_AUDIO_OUT_TransferComplete_CallBack(), BSP_AUDIO_OUT_HalfTransfer_CallBack() and DMA1_Stream0_IRQHandler(), but none of them seems to be called when using debugger.

Would you have an advice or a hint ?

Thanks,

PE

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0