cancel
Showing results for 
Search instead for 
Did you mean: 

Repeated start with HAL drivers on STM3273C

AEsca.2
Associate

Hello, 

I am using the STM3273C board as an i2c slave. The master is requesting the data via repeated start.

For this I am using the method HAL_I2C_Slave_Sequential_Transmit_IT. The problem is that the first byte after the restart 

is always 0xFF. The data starts to be filled from the second byte.

Could somebody please point me in the right direction please?

Thanks in advance,

Ana

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amira
Associate III

Hello @AEsca.2​ 

Can you please indicate which STM32F3 firmware version you are using.

Regards,

Amira