Skip to main content
antonius
Associate III
January 23, 2019
Question

Reading ADC ?

  • January 23, 2019
  • 3 replies
  • 676 views

Dear ST Community Members,

I want to read a value from 2 ADC channels on STM32L031,

How can I do that using polling conversion ?

Thanks

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
January 23, 2019

Spin in a loop waiting for the content of the DMA buffer to change?​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
antonius
antoniusAuthor
Associate III
January 23, 2019

Thanks Clive for the answer,

My code already with poll conversion, how can I separate ADC_result from CH0 and CH3 ?

ADC_raw = HAL_ADC_GetValue(hadc); 
 
How can GetValue(hdc) CH0 and CH3 ?
 
currently I comment out one of the setting :
 
static void MX_ADC_Init(void)
{
 
 ADC_ChannelConfTypeDef sConfig;
 
 /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) 
 */
 
 hadc.Instance = ADC1;
 hadc.Init.OversamplingMode = DISABLE;
 hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
 hadc.Init.Resolution = ADC_RESOLUTION_12B;
 hadc.Init.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
 hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc.Init.ContinuousConvMode = DISABLE;
 hadc.Init.DiscontinuousConvMode = DISABLE;
 hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc.Init.DMAContinuousRequests = DISABLE;
 hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc.Init.LowPowerAutoWait = DISABLE;
 hadc.Init.LowPowerFrequencyMode = DISABLE;
 hadc.Init.LowPowerAutoPowerOff = DISABLE;
 if (HAL_ADC_Init(&hadc) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 /**Configure for the selected ADC regular channel to be converted. 
 */
 
	sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 /**Configure for the selected ADC regular channel to be converted.*/ 
 
 //sConfig.Channel = ADC_CHANNEL_3; //comment out for reading only one ADC
 
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
}
 
on the callback :
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
 if (__HAL_ADC_GET_FLAG(hadc, ADC_FLAG_EOC)) 
 { 
			ADC_raw = HAL_ADC_GetValue(hadc); 
			
		//	HAL_GPIO_TogglePin(OUT1_GPIO_Port, OUT1_Pin);		
			
			if(Index < 100)
			{
			//	HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET);
				ADC_Cplt = 0;				
				Value[Index] = ADC_raw;
				Index++;
			}
				
			else
				{
					ADC_Cplt = 1;
				//	HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
				} 
		
			
 } 
}

Any ideas ?

After Forever
Senior III
January 23, 2019

Try to follow the example projects from Cube. Then if you have questions, you can ask here.

Install STM32CubeMX, download and install the STM32L0 package from the there (Alt+U).

Open Help->Updater Settings (Alt+S). [Click Show More to see the whole post]

Press the Browse button next to Repository Folder box

For HAL example project, go to STM32Cube_FW_L0_V1.11.0/Projects/NUCLEO-L031K6/Examples/ADC/ADC_RegularConversion_Polling

For LL example project, go to STM32Cube_FW_L0_V1.11.0/Projects/NUCLEO-L073RZ/Examples_LL/ADC/ADC_SingleConversion_TriggerSW