2025-12-31 8:11 AM - last edited on 2025-12-31 8:17 AM by Andrew Neil
Hello, I am getting really frustrated with this issue for almost a week.
I am trying to read PA1 and PA4 in DMA but I get only the reading of one channel and not the other one! I tried everything and I also looked at all the example online. Please help.
Solved! Go to Solution.
2025-12-31 8:58 AM
> I get only the reading of one channel and not the other one!
Why do you think that is the case? What readings do you get and what do you expect instead? Be specific.
> uint32_t adcValues[100]
> hdma_adc.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
This should be an array of uint16_t, not uint32_t.
2025-12-31 8:58 AM
> I get only the reading of one channel and not the other one!
Why do you think that is the case? What readings do you get and what do you expect instead? Be specific.
> uint32_t adcValues[100]
> hdma_adc.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
This should be an array of uint16_t, not uint32_t.
2026-01-01 8:27 AM
Hello TDK,
thank you for your interest.
I think there are some mistakes in my code (that's why I shared the 3 main files). If someone can be so kind to have a look or suggest a working example to look at.
in my array I get:
adcValues[0]= 200 ,
adcValues[1]= 0 ,
adcValues[2]= 190 ,
adcValues[3]= 0 ,
adcValues[4]= 201 ,
adcValues[5]= 0 ,
and so fourth ...
2026-01-01 9:25 AM
Did you correct the error I noted?
2026-01-11 7:25 AM
Thank you the DMA works good. thank you