cancel
Showing results for 
Search instead for 
Did you mean: 

problems with usb msc device on stm32f4

MishaT
Associate II

Hi. I need to create USB MSC Device on STM32F407. I use CubeMX for create project. When I compiled the project with MSC_MEDIA_PACKET = 512 windows did not see the mass storage device, then I changed MSC_MEDIA_PACKET = 256 and windows saw the mass storage device and also offered to format it. I also did projects on stm32f0 and stm32f3 with MSC_MEDIA_PACKET = 512, everything worked without problems for them, Windows found the device and offered to format the disk. How to do when define MSC_MEDIA_PACKET = 512 for Windows to see it?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0